Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
Dear ST community, I have 2 Nucleo WL55 highband boards and I suspect that there has been a mislabelling of the device. As I am aware of, only the D-04 version of this board is sold. However, my board has several pins that do not correspond to the ones mentionned in the datasheet. By looking closely at my device, I see that the sticker label mentions the D-04 version, however, on the PCB itself I see D-01 (see image below). Is it possible to obtain the User manual and schematic for this version of the board? I cannot find it anywhere and it is really painful to probe each pin to reverse engineer the PCB connections. Thanks in advance, Balazs Udvarhelyi
I'm trying to get started using the STM32WLE5-series chip, and I'm really struggling to figure out how to get the `AT` firmware example going. I see it in the SDK package, but it's only for the STM32WL5-series (dual-core) chips. I see this setting in the .ioc file, but it doesn't tell me how to get to the Examples List?Thanks!
STM32CubeMonRF: https://www.st.com/en/development-tools/stm32cubemonrf.htmlSeems to apply to BLE and IEEE 802.15.4 only?Is there anything similar for sub-GHz ?
I need more flexibility in my project(s) and I have now left the Arduino-world for a new hardware design around the STM32H7.Two general questions:Are there any resource libraries covering useful C-drivers for commonly used sensors or displays? Like simple IMU:s, temperature and smaller displays.Does ST has any best-of-practice recommendation for a STM32-board design with a Wi-Fi connection? For instance, I am considering the Murata LBEE5KL1D (Wi-Fi + BLE) which is currently used on the Portenta board.Thanks in advance
Hi everyone,I'm currently trying to build a lora project with I-Cube-LRWAN v2.0.0 and CubeIDE.I've been able to use the "End Node" example as-is but a can't include the library in a CubeMX project.My goal is to have the .ioc file and the library in the same project. This way, I want to be able to add peripherals to the project with the .ioc. (ADC2 for example)It seems that the newer version of the library have been made for this purpose but I can't make it work.I'm using a Nucleo-l476rg and sx1276mb1mas board.Do you guys have any idea ?Thanks in advance
I think I got the setup for the Real-Time-Clock (RTC), but how do I verify it is working?Is there a way to output the timestamps or check through a file? I am using the STM32WB55 Nucleo Board, and currently using the STM32 IDE.
or if I must write my own code, how to do itThank you,
Is it possible for stm32WB to recieve audio from a mobile device via bluetooth and at the same time send the audio to another device like headphones or wilreless earphones via bluetooth .Reception and Transmission should work simulteneously.Does it suppourt this ?
Does the STM32WB have drivers to support serial communication over it's USB port?
1081s730:MAC txDone<CR><LF>02-05-2021 23:17:35.489 [RX] - 1082s751:RX_1 on freq xxxxxxxxx Hz at DR 0<CR><LF>1082s958:MAC rxTimeOut<CR><LF>1083s715:RX_2 on freq xxxxxxxxx Hz at DR 2<CR><LF>02-05-2021 23:17:36.528 [RX] - 1083s791:MAC rxTimeOut<CR><LF>
Hi, Working with FW_WB_V.10.0, have a few questions:After viewing the workshop tutorial, I saw multiple code insertions to the project. (https://www.youtube.com/watch?v=zNfIGh30kSs). Are they necessary?Started working with FW_WB_V.10.0, can I safely upgrade to FW_WB_V.11.0/1? What are the differences? And is it somehow related to my previous question?In cubeMX, in the custom BLE example and in general, can we change the names of the services and characteristics from inside the cubeMX? To be later generated to code? This can save tedious name changes and functions in codeThanks
Hi everyone,STM32WB5MMGH6TR has DXF/3D or CAD files for design?I use Kicad more often for designOliver
..
I have a custom board with a STM32WB55 that is getting stuck in the sequencer and stops executing as soon as I start my code. I can't tell if it's a race condition and I don't have the ability to step through the code with a debugger. The code is basically just a slightly modified version of the Nucleo Heartbeat code example. Running stm32wb5x_BLE_Stack_full v1.11.1. Here's my main():int main(void) { /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* Initialize all configured peripherals */ MX_GPIO_Init(); /* Configure the system clock */ SystemClock_Config(); //Init_Exti(); MX_IPCC_Init(); MX_RTC_Init(); /* Init code for STM32_WPAN */ APPE_Init(); UTIL_SEQ_Init(); /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ UTIL_SEQ_Run( UTIL_SEQ_DEFAULT ); /* USER COD
Does anyone have an experience with binary open source solution from Stackforce? Is it a .a library for gcc linking?
I have read different articles of STM and received different mails to use TCXO to give 32MHz clock. I could not find the reason and impact of it. In my application, it is outdoor and able to go temperature upto 85C temperature and using 22dB with 865MHz and its low power device.My questions are:1- If i use normal crystal of 10PPM (frequency tolerance and stability), what is the issue? what is the drift i can expect in clock and how it is going to impact the RF communication or any other place in MCU?2- what is the PPM budget defined for STM32WL? (referred AN2867)3- i have choosen below crystals, kindly confirm, which one can i use ?ECS-320-8-37B-7KY-TR ECS Inc. | Crystals, Oscillators, Resonators | DigiKeyECS-320-10-37B-CKY-TR ECS | Mouser IndiaECS-320-8-36B-CKY-TR ECS | Mouser IndiaECS-320-8-47B-7KY-TR ECS Inc. | Crystals, Oscillators, Resonators | DigiKey 4- if i have to use TCXO only, can i use below part as used part in nucleo board is not available?TG2520SMN 32.0000M-ECGNNM3 Epson
Hello,I have read the datasheet/reference manual on stm32WL generic format, i also looked into the cube wl sources. From the source codes i understand that stm32wl integrates semtech sx162x radio. I have not been able to pinpoint anything more specific about the radio than this. (at least i didnt find semtech radio that can do bpsk)The question is about generic packet format - all semtech devices have FSK format (variable length) as :preamble+syncword+length+address+payload+crcThis packet looks very very compatible with existing solutions (eg from TI.com)BUT!in stm32wl reference manual this format is presented as:preamble+access address+packet length + 1 BIT + payload + CRCCould someone knowledgeable comment on this ? (someone ST related) Because to me it looks that datasheet is wrong. Or ST added single bit just to be incompatible with everything that is currently being used on the planet. Or i dont know.
I am using an STM32WB55CG in a slightly challenging environment. aci_gatt_update_char_value() works great most of the time and returns BLE_STATUS_SUCCESS and transmits data. Occasionally the STM32WB55CG will disconnect and then reconnect. Our application continues to call aci_gatt_update_char_value() which still will return BLE_STATUS_SUCCESS but no data is transmitted. If our unit disconnects and reconnects again, the STM32WB55CG will once again start transmitting data.If aci_gatt_update_char_value() returns BLE_STATUS_SUCCESS is there some other way for us to know if the transmission was successful?When we are in this mode, this is the only packet that the STM32WB55CG sends.
Hi,We are working on a application using the STM32WB55 and are using the P-Nucleo boards. We want to have multiple (5-8) servers connected to a single client and with a low latency and the highest throughput possible.All servers are sending data with Notifications, both DLE and 2M is enabled.From the testing we have done it seems that the Client gathers data from one client at a time. With 5 servers and 7.5 ms connection interval it results in a minimum latency of 30 ms, which in our case is too high. This also splits the throughput in half for each server connected.Is it possible to have a system like the one proposed here on the Nordic Forums? https://devzone.nordicsemi.com/f/nordic-q-a/44762/ble-multi-link-high-throughput-lowest-latencyNordic claims that it can support at connection event of 2.5 ms which results in data from 3 different devices in a connection interval of 7.5 ms.Do you have a minimum connection event length? and is it possible to receive data from multiple servers t
I am developing the BLE application on my custom PCB using MCU STM32WB55CCU6. However, it gets stuck in if (SHCI_C2_BLE_Init( &ble_init_cmd_packet ) != SHCI_Success) { Error_Handler(); }It returns SHCI_FUS_CMD_NOT_SUPPORTED instead of SHCI_Success so it jumps into the Error_Handler(). I tried to flash the FW into the nucleo board. It works perfectly fine. But it failed to initialise the BLE stack on my custom PCB. Therefore, I think it should be the hardware problem. I checked HSE and LSE clk. They are initialised successfully and the waveforms can be observed in CRO. I am sure that they are oscillating. Can anyone give me some advise on this issue? Thank you very much
I would like to add middleware (LoraWan, SIGFoxor subGHz_phy) but those are disabled and when I hover my mouse on enable I get the tooltip saying "you can enable this middleware only if SubGHz is enabled..".When I open examples these middleware are active? any help?
I generate project using CubeIDE 1.6.1 with pack 1.11.0 for stm32wb55CC. I select BLE in code generator and look at Debug options. But it looks this options value not matter. I create project with enabled and disabled debug options and compare .c and .h files and no different... Please fix this problem. @Nawres GHARBI
Working on STM32WB50P2P server client (one to one) working perfectly. Server sends notification which is 240 bytes long.Shifted from Client to router to connect to multiple servers and transfer collected data to an Application.In router application was able to connect to multiple servers but notification was being received from only one server.More testing revealed that sometimes data from multiple servers was being received.Further testing revealed that if delay is introduced in the function:aci_gatt_write_char_desc(aP2PClientContext[index].connHandle, aP2PClientContext[index].P2PClientDescHandle, 2, (uint8_t *)&enable);then notification is received correctly.Our assumption is that the software is designed to allow the connection of servers one by one. But since our servers are in advertisement mode all the time, they connect to the router immediately.Our code looks like this now: case APP_BLE_ENABLE_NOTIFICATION_DESC: APP_DBG_MSG("* GATT : Enable Server Notification\n
Hi everybody, I'm a student in a French engineering school currently working on a project including the STM32WB wireless CPU series. For the sake of simplicity, I'm just going to say that my project basically consist in establishing a BLE connection using a 1000 µF capacitor as my only energy source. Here comes my question : I've tried using the "Low power manager" that comes with the sequencer when generating the code trough CubeMx : I've enabled it in app_conf.h aswell as disabled all debugging options and made sure it was configured for the StopMode2. My understanding is that my STM32WB should enter StopMode between 2 advertising packets, so if I monitor the consumption , I should be able to see it drop to a couple µA when in StopMode and rising back up for a very short time everytime a packet is sent. However, when configuring the advertising to send a packet every 5 secondes, my energy comsumption do not drop to a couple µA after sending the first packet. My guess is
Namaste,I am working with a full-duplex audio streaming application using the project files given here: https://www.st.com/en/embedded-software/fp-aud-bvlinkwb1.htmlI am using the STM32WB Nucleo board and the code works where I can play the audio file using an ST BLE sensor app. The audio file will be recorded on the laptop using Audacity software. The Nucleo board will stream the audio received over BLE and sends it to the laptop over USB. The Nucleo board is shown as an audio input device. I want to play the audio received by the Nucleo board using wired speakers connected to it. For this, I need an audio DAC which uses I2S and I2C communication for the interfacing. Now I need an evaluation board to see if it works before I can go ahead with the hardware design. Can anybody guide me about this? The hardware must play the BLE app's audio and send the mic recorded audio back to the app in real-time.Thank you.
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.