Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
Does anyone know if there is a table or some reference which shows how many bytes each binary will consume on the target STM32WB's Flash memory?
We have STM32WL working well on LoRa together with Teseo-liv3f Nucleo boards. We now need to have it to sleep for low power between tasks.Our software is based on the LoRaWAN_AT_Slave example. In there we can allow everything to go into sleep mode 2. Hwever we find that after coming out of sleep mode the I2C bus used for the Teseo-liv3f remains in a busy state, the clk and data lines are both high so not busy, we have also tried a delay before access but still no go. Are there any issues with this?
I have the STM32WL LoraWan_End_Node example working, but I don't understand the code with UTIL_SEQ_Run(UTIL_SEQ_DEFAULT); Where can I change the payload to send an ADC value to TTN?
..
As dragino lg02 is able to transmit the packets just in 1 frequency e.g. 868200000 would you please clarify the steps for prototyping wl55c-lorawan-endnode from the beginning to end with cubeIDE for the single channel GW ?
Hi all,Im using the STM32WB as client to send some measurement data to my phone or pc application. Communication works fine and now I'm trying to reduce the power a bit and want to change the connection interval to high when I'm sending much data.I'm using the call aci_l2cap_connection_parameter_update_req() from task context as shown in p2pServer example (STM32CubeWB-1.9.0) . I notice in the p2pServer example that when connected to my phone and I press the btn2 to update the connection interval it will not always call the " EVT_BLUE_L2CAP_CONNECTION_UPDATE_RESP " while the change seems to be applied (looking with STM32cubePowerMonitor). But the mutex is not reset, meaning the connection cannot be reset again.For now instead of a mutex I used a delay that's long enough to apply the change. Which is ok for the mobile andriod app "ble scanner" (i can see on power monitor the interval change and get all the data) .However my pc application (working with a bluegiga dongle) does apply the c
I'm debuging thread application(On P-Nucleo with STM32WB) in order to know how thread core manages adresses, but when i start to debug, the program starts to be flashed on the board,and i can't even know how adresses are maneged. Can anybody help me about this issue ?
Hi,The AN5185 in "FUS upgrade" part says that FUS can be updated even with wireless stack installed. According to release notes start address for FUS should be 0x080EC000, but if a wireless stack is installed (for example BLE) this area will be locked (SFSA will be 0x080ca000). So, do we need to delete the wireless stack before FUS installation?
Hi everyone. I'm new to STM32WB and using P-NUCLEO-WB55. I wonder that how can i scan ble device near by and read their rssi. Can any body show me the way. Sorry for my bad english.
I'm developing LoRa's ENDNODE using the "ENDNODE" example.In the "ENDNOE" example, see "AT_SLAVE" to run ATCOMAND.For UART setupTo change to UART2->LPUARTextern UART_HandleTypeDef hlpuart1;I'm developing LoRa's ENDNODE using the "ENDNODE" example.In the "ENDNOE" example, see "AT_SLAVE" to run ATCOMAND.For UART setupextern UART_HandleTypeDef hlpuart1;I'm developing LoRa's ENDNODE using the "ENDNODE" example.In the "ENDNOE" example, see "AT_SLAVE" to run ATCOMAND.For UART setupTo change to UART2->LPUARTextern UART_HandleTypeDef hlpuart1;I'm developing LoRa's ENDNODE using the "ENDNODE" example.In the "ENDNOE" example, see "AT_SLAVE" to run ATCOMAND.In main.h for UART setupextern UART_HandleTypeDef hlpuart1;#define UartHandle hlpuart1Declared thatAt uart_if.cUTIL_ADV_TRACE_Status_t vcom_Init(void (*cb)(void *))void MX_LPUART1_Init(void)You have also added an msp function.Add a functionstm32l0xx_it.c에 "void LPUART1_IRQHandler(void)"I also added a handler.However, neither the applog
Hello! I've been working with the STM32WB55 Nucleo development board for a while and it looks like when it was setup, it was setup for 512 kB of flash, though all documents online seem to suggest it should have 1M of flash. The chip on the development board is an STM32WB55RGVx (VFQFPN68). According to this link, it does have 1M of flashhttps://www.st.com/en/microcontrollers-microprocessors/stm32wb-series.html#productsI initialized it in STM32CubeIDE in pack 1.3 originally, so maybe this is an outdated issue? Regardless, this is what it shows in my linker file:/* Specify the memory areas */ MEMORY { FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 512K RAM1 (xrw) : ORIGIN = 0x20000004, LENGTH = 0x2FFFC RAM_SHARED (xrw) : ORIGIN = 0x20030000, LENGTH = 10K }Based on this, I assume I should be able to just change 512K to 1024K, clean, and rebuild but I thought I'd check in here and find out:1) Is it as simple as changing the code from 512K to 1024K and I'm ready to go or is there a reason it's s
I'd like to use the Nucleo example with a different MCU. Is there an built-in tool for this?
Hi,I'm using the STM32WB5M Discovery kit and I'm integrating the USB-VCP library with th power control. After the wake-up from the STOP 1 Mode the USB-VCP doesn't work (I don't receive the characters send using the function CDC_Transmit_FS), after some tests I resolve adding MX_USB_DEVICE_Stop() before to go into stop mode and adding MX_USB_DEVICE_Start() after the wake-up. Is it correct? Does it Exist some other procedure to manage the USB-VCP with the STOP 1 Mode?With this configuration I can't wake-up the MCU sending character throught the VCP, how can I resolve?Regards,Giampietro
Hey guys,Im running into some issues with trying to set the clock speed of my stm32wb55 chip above 32MHz on my custom board.Here is my baremetal startup code that works using MSI as sysclkvoid __attribute__((naked)) Reset_Handler() { __asm__("ldr r0, =_estack\n\t" "mov sp, r0"); // Copy data section from flash memory to ram uint32_t data_section_size = _edata - _sdata; memcpy(_sdata, _sidata, data_section_size*4); // Zero out bss uint32_t bss_section_size = _ebss - _sbss; memset(_sbss, 0, bss_section_size*4); // Set Interrupt Vector Table Offset SCB->VTOR = (uint32_t)interrupt_vector_table; rcc_reset(); RCC->CR &= ~(RCC_CR_MSIRANGE); // RCC_MSI_CLOCK_SPEED_32MHz = 0xa RCC->CR |= RCC_MSI_CLOCK_SPEED_32MHz << RCC_CR_MSIRANGE_Pos; main(); }However if I change line 20 to this:// RCC_MSI_CLOCK_SPEED_48MHz = 0xB RCC->CR |= RCC_MSI_CLOCK_SPEED_48MHz << RCC_CR_MSIRANGE_Pos;My program will refuse to run. Trying to step throu
hello, I downloaded Subghz_phy_pingpong example and i opened the project file.Then i opened main.c . it looks like in the picture below. i think its empty or did i opened in wrong way?
I am trying to make the make the thread command line application on my custom board that communicates through the usb. In the WPAN configuration in CubeMX there does not seem to be an option that turns on CFG_USB_INTERFACE_ENABLE. Does anyone know how to turn this on?
Hi all,I have the STM32WB55 board connected to a battery. However it loses connection (firmware does continue without issues) quite often. After some research I have found out that when i attach the charger or the st link the disconnection issue is gone. Leading me to believe that the battery isn't capable of supplying enough for the system + ble when transmitting.So I've added a 36uF polarized capacitor on the 3v3 of the arduino morpho connector to provide for the peaks. This does solve the problem as well.Now the question:How big a capacitor do I need to be able to transmit data without losing connection? In the UM2435 user manual stm32wb are some power related schematics. The 5v has a 10uf +100nf and the 3v3 has 1uf and few 100nf....My hardware knowledge is not good enough to determine the size I need, please help.Kind regards,Taxara
Hello!Is there an overview of how big the ST wireless stack is depending on the activated features?Thank you!
Hi,I have P-NUCLEO-LRWAN2 starter pack and I'm trying to run AT Master application on NUCLEO-LRWAN1/NUCLEO-L073RZ pair with supplied in I-CUBE-LRWAN Expansion Package. It looks like all fine (i.e firmware compiled and loaded onto NUCLEO-L073RZ without any problem). But GW cant get any data from the Sensor Device. Finally, when I checked with SDR , I cant see any Tx activity from the Sensor device .. I will be so happy if you can make comment on this. many thanks in advance, reha
I bought p-nucleo lrwan2 working with STM32LO MCU,and i'am wondering to configure its device sensor as end node ,watching the last video posted by ST they were working with the same pack but they targered STM32WL as end node instead of working with the STM32LO.
This is the only code I could find. There is no information about which device this can be used with either. please help me
I want to use software uart in NUCLEO-WL55JC2.
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.