Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
Dear Community,I'm using a P-NUCLEO-WB55 Board and Dongle, until now only with ST examples.I'm trying to perform firmware update using BLE OTA (switching from BLE_HeartRate_ota to BLE_p2pServer_ota for example) and am facing a problem.The same problem appears if I Use STM32 CUBE Monitor-RF on PC with P-NUCLEO Dongle or using STM BLE Sensor App on Android smartphone.Here is my issue:I can find my device and start an OTA update.Flashing starts and very frequently, it suddenly stops, like if connection was lost.I checked, I have a stable power supply.Could you please give me any hint on how to proceed for debugging?Thanks and best regards
Hi. I am Jay working with STM32 ST board (MB1355C and USB dongle) to build Zigbee application. To become familiar with STM32Cube Firmware, I picked and ran one example of STM32Cube_FW located at STM32Cube_FW_WB_V1.13.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\Zigbee\Zigbee_SE_Msg_Server_RouterSTM32Cube_FW_WB_V1.13.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\Zigbee\Zigbee_SE_Msg_Client_CoordI used Nucleo board and USB dongle for Coordinator/Router each. When I do coverage testing (i.e possible distance), I found that Router (USB dongle) succeeds in joining Coordinator within 8~10m distance. While trying to increase Tx power with using "ZbNwkIfSetTxPower()", I found that "APP_ZIGBEE_NwkForm()" sets Tx Power to 0dB (default value). Due to its setting Tx Power value to 0dB, I should put a Router (USB dongle) within 8~10m away from Coordinator. I dig out more into "ZbStartup()", I cannot find how to set Tx Power in that function. Actually I want it to form a Zigbee networ
..
I've hit the limit of my research and don't have any experience writing to flash other than at compile time using the keyword 'const', but that doesn't help me because I need to be able to continuously write data. I have a very basic and general sense of what a page and bank is, and just need some help getting started trying to find out how to go about doing this. I'm trying to implement a double buffering mechanism, but to have it stored in flash because my application does not have enough RAM to dynamically allocated what it needs during the worst case. I simply need to write 8-bits of audio sample data in two buffers at 8khz, so every second, I need to be able to page in one second's worth (8 KB) of samples to process while DMA is writing to the other 8 KB buffer. Is this even possible?I don't understand what it takes to be able to erase a bank and write to it, but I feel like it might be complicated, and I'm willing to learn. From what I hear, the read/write cycle is slow, but I'm
HI all,I’d like to create a system communication using LoRa protocol between 2 devices, I don’t want to use TTN. I’m newbie with LoRa I’ve seen Seed provide SDK to use LoRaWAN but I don’t want to use gateway or server. To be simple I have one device with LoRa-E5 and another device with another LoRa-E5, I’d like to be able to comunicate with LoRa between those devices, so it is End device to End device I think, is it possible ?
So, I have TIM2 setup to trigger an ADC conversion and the DMA moves the samples out to RAM. I want to do this every 100us for 1000 iterations. Sounds pretty straight forward. There are 3 ADC channels being sampled using the sequencer on every trigger, so 3000 samples total. Everything works except for the timing. I turned on the timer interrupt and I am only getting to around 600 interrupts when the DMA reports that all the samples have been transferred. I expect there to be 1000 timer ticks. It seems like the ADC is not getting triggered on the timer interrupt, but on something else. Ive tried a lot of configurations and it never seems to change the outcome. Im stumped... Micro is the STM32WB55Timer setup:SENS_Tim2.Instance = TIM2; SENS_Tim2.Init.Prescaler = ((SystemCoreClock / 1000000u) - 1u); // Scale input clock to 1mhz SENS_Tim2.Init.CounterMode = TIM_COUNTERMODE_UP; SENS_Tim2.Init.Period = ((1000000u / SENS_PUMP_SAMPLE_FREQ) - 1u); SENS_Tim2.Init.ClockDivision = TIM_CLOCKDIV
Hi all,I've been trying to use the STM32WB55 Dev Kit and if I generate the project with the peramitirs below and then try to build the project I get this error;*** Error Code *** C:/Users/bryce/STM32CubeIDE/workspace_1.3.0/STM32WB55-MB1355C/Debug/../STM32_WPAN/App/app_thread.c:582: undefined reference to `MX_LPUART1_UART_Init'I'm not too sure how to debug this, please could someone help me with debugging this issue.I think its todo with the GUN not being able to see the Utilities folder?*** Project Config *** HSEM -> Active RF -> Active RTC -> Active LpUart1 -> Mod -> Asynchronous STM32_WPAN -> Thread -> Active STM32_WPAN -> Thread -> Configuation (Tab) HW UART -> CFG_HW_LPUART1_ENABLED -> Enable App Parameters -> CFG_CLI_UART -> hw_lpuart1 Clock Configuration -> Resolve Clock IssuesThanks for looking into this and if you need anything Please let me know
Hi St forum I'm in the progress of creating a peripheral BLE application using the STM32WB55CE on a custom board. I'm trying to implement low power now, but struggling.. Using the X-Nucleo-LPM01A power monitor board I've measured my current consumption (no low power implemented): This is not impressive, but expected. To get a grip on ST low power, I've run various examples on the P-Nucleo.WB55 dev. board, but it looks like the current consumption is very high no matter the example??? I've based my guesses on the Power features application note. Setup: All jumpers from STLINK is removed during test. PWR_STOP2_RTC exampple: expected ~2.2uA PWR_EnterStandbyMode: expected < 1uA. PWR_SMPS_16MHZ_HSI w/o RF Stack: ?? PWR_SMPS_16MHZ_HSI with RF Stack: BLE_HeartRate: not sure. So the question is: I'm I missing something vital? Ideally I would like the application to enter either STOP2 or STANDBY when no BLE central
In STM\STM32Cube_FW_WL_V1.2.0\Projects\NUCLEO-WL55JC\Applications\LoRaWAN\LoRaWAN_End_Node\LoRaWAN I cannot find an explanation for the NUCLEO-WL55C1 LEDS GREEN, BLUE, RED meanings. In lora_app.c I found: AppLedStateOn = appData->Buffer[0] & 0x01; that toggles the RED LED There is nothing in the DOCS, README, PDF files and the source is not commented to the programmers intentions, must be real obvious but I'm missing it.
We want to transmit audio over Bluetooth.We are new to audio and Bluetooth. We have got P-nucleo-WB55 board for Bluetooth and ST EVAL MIC007V1 sensor for digital audio.Can anybody guide us with an example project using I2S.Thanking in advance.
Hey,unfortunately the dongle is no longer recognized as a serial port when i load one of my projects onto the device. When I use the example applications, it works fine. Any idea what this could be.Thanks in advanceEddy
Errors occurred during the build.Errors running builder 'CDT Builder' on project 'EN_Silva'.A resource already exists on disk '..../Debug/sources.mk'.A resource already exists on disk '..../Debug/sources.mk'.A resource already exists on disk '..../Debug/sources.mk'.A resource already exists on disk '..../Debug/sources.mk'.Any idea?Also, I cannot create Debug configurations -- the entries vanish from the list when opening the dialog next time..Thanks!
Hello,I am having issues with RTC Alarms in BLE applications on my STM32WB boards. If BLE isn't turned on, the alarms work correctly. When I turn BLE on, the alarms stop working. After some debugging, I found out that the RTC registers are set up correctly, and the alarms trigger their respective hardware interrupt flag, but for some reason RTC_AlarmIRQHandler doesn't get executed. This behavior happens in both my custom BLE application and the example BLE applications CubeMX can generate. Does anyone have any tips what the issue might be? Thanks.Edit: Forgot to mention MCU types: one board has a WB50CGU, the other one a WB55CGU.
Hello,I'm trying to auto generate the the AppKey on device boot using the KMS Derive.I have enabled the LORAWAN_KMS definition as described on the AN5406 and also the configuration that needed. But the device don't generate any key and after investigation the C_DeriveKey() throwing error CKR_DEVICE_MEMORY that cant find a solution yet. Is any better way to auto generate the key without flashing any blob?Using the stm32wle5 mcu
Hello,I have started to develop one LoRa end node around a STM32WLE5CC6 chipset(QFPN48).My device is operating in EU868 band. While the device is transmitting, I acquire the data for the frequency spectrum with a spectrum analyzer. As you can see from the screenshot, there are unwanted sided-signals(spurious) around the central frequency(868 MHz). Specifically, both the lower side and the upper side are equally away 5 MHz from the central frequency.What is your consideration for the possible root cause of spurious injection? Is there any way to block or reduce these spurious?Thanks in advance,Stavros.
Hi,Currently, I'm working with the P-NucleoWB55 evaluation kit, and I'm developing a Zigbee network to exchange some messages between devices. My problem comes when I have to form and join the network. I'm not sure about the meaning of the configuration parameters: panId, networkManagerAddress, extendedPanId, shortAddr. I would like to know what are those parameters useful for (form the network, join, and identify the device).
I am using STM32WB Discovery kit for STM32WBB5MM MCUs for development. I've setup the board as a RFD, Centralized End Device. How do I disable Zigbee security level if I don't need it? Currently, I have to set it manually in APP_ZIGBEE_NwkForm() by config.security.level = 0;However, this would get erased once I regenerate the code with STMCubeMX.Thanks in advance for any help.
Hello, I would like to use the NUCLEO-WL with Sigfox and LoRaWAN in the code as proposed in the workshop (youtube video : MOOC - STM32WL workshop - 6 LoRaWAN and Sigfox coexistence). However, the zip project is not part of CubeWL. Thus, How can we update this project with the new version of CubeWL (1.2.0) ? Or, how can we create a Sigfox/lorawan coexistence directly from the CubeWL 1.2.0 ?Maybe @Bartosz BORYNA or @Szymon PANECKI (employees in charge of this workshop) have an answer (?)Thank you Best regards
Hello ST Community,I want to know if the STM32WB55RG supports MAC 802.15.4 Beacon Mode.For now, I'm sure that the CM0+ Stack supports Only the Non Beacon Mode (SO=BO=15) and Full broadcast Mode (PANID 0xFFFF, dest @ 0xFFFF) and OFC doesn't support PIB security model defined by the standard.I have tried to enable the Beacon mode but no luck.I always end up with a 0xC0 status when trying to send Data and my sniffer catches nothing ( no beacons are sent nor Data ).Can somebody please confirm that the Stack doesn't support Beacon Mode ?Regards,
I am currently using 2 STM32WB55RG MCUs and they are currently running the ZigBee_OnOff example project. Unfortunately, they are not working due to this error message that I see on a HyperTerminal:"RF IF return CCA or CSMA issue!".I'm not sure what is wrong and I have not edited the example project code. I have flashed the appropriate firmware to the MCUs as well.
[Deprecated]
Hi all,I'am working with LORA and LORA-E5 chip, I'am trying to adapt the ping pong stm32 example (without lorawan). But for now I have a question, I'd like to have a point to point application, but my question is can I set a server and a client address ? I wan my 2 devices comunicate only between they.
Hi,I try to launch the demo application called Zigbee_DoorLock_Server_Coord on a nucleo board WB55 with GDB and I have an error "Error on final launch" Device Debug Script (cf image)Others applications are OK.The application can run without GDB (RUN mode).I have the same behaviour if in my project I add : zigbee_app_info.time_server = ZbZclTimeServerAlloc(zigbee_app_info.zb, TEMP_ENDPOINT, &ZbZclTimeServerCallbacks, NULL);ZbZclTimeServerAlloc function can be the problem in debug mode ?ThanksAnthony
Hi,I'm working with the BLE p2p-Router project and added the discovering of a Health Thermometer service. It works ..., but the discovering of the descriptor of the termometer measurement characteristic gives an unexpected answer. I use the start & end handle of the discovered characteristic to start the discovering of the descriptor and the answer is equal to the end handle of the characteristic. Perhaps ok, but the UUID that is given with the "ACI_ATT_FIND_INFO_RESP_VSEVT_CODE" event is also equal to the characteristic UUID. I would expectthe UUID 0x2902. If i discover the same server module with a similar project of another manufacturer i get the correct UUID of this descriptor.I'm asking, because i can't activate the indication of the temperature measurement with my application (i use the aci_gatt_write_char_desc() with the handle i received during discovering)Thanks for your helpNicolai
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.