Associate
Feb 8, 2021 12:53 PM UTC
Question
Zigbee_DoorLock_Server_Coord Application in DEBUG mode
- 2 replies
- 1185 views
Hi,
I try to launch the demo application called Zigbee_DoorLock_Server_Coord on a nucleo board WB55 with GDB and I have an error "Error on final launch" Device Debug Script (cf image)
Others applications are OK.
The application can run without GDB (RUN mode).
I have the same behaviour if in my project I add :
zigbee_app_info.time_server = ZbZclTimeServerAlloc(zigbee_app_info.zb, TEMP_ENDPOINT, &ZbZclTimeServerCallbacks, NULL);ZbZclTimeServerAlloc function can be the problem in debug mode ?
Thanks
Anthony