TODAY | STM32 Summit 2026
Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.
Most recent activity
Hi ,I am coding for STM32F207 for first time so I do not understand Why is STM32F207 processor loading 16 bit thumb instruction where as the Function pointer is 32-bit . is this ((void (*)(void))g_ulTransferAddress)() wrong ? As per our Project requirement we have 4 different sections of 1MB Flash. All the 4 Different sections of 1MB flash has 4 independent projects.1. CRC Verifier Project 0x0800_0000 to 0x0800_3FFF2. Decision Maker Project 0x0800_4000 to 0x0800_7FFF3. Bootloader Project 0x0800_8000 to 0x0801_FFFF4. Runtime or Scheduler Project 0x0802_0000 to 0x0810_0000Decision Marker should be loaded from the CRC verifier for this I am using following code g_ulTransferAddress=0x0800_4004 ;
SBSFU considers the secure boot as the root of trust. If we develop the firmware and manufacture the products in a factory (I assume that the firmware should be programmed during the manufacturing in the factory), how to guarantee the secure boot is correctly programmed? Any guideline for a good practice? Thanks!
I have a large application image running on the STM32F427. The image is more than 1M bytes, which make it impossible for dual-image. From ST's document, for single-image, "The user application cannot download a new firmware image: the local download procedure is the only way to update the active user code."One solution is to download the new image to external flash or SD card, what is the problem with this solution? If it is not a good idea, and I want to download the new firmware via OTA, then I have to implement the OTA code in SBSFU project?Or any suggestion?Thanks in advance!
i want to get the stm32 cryptographic library and i request it. but after a week no response received. what should i do?please help me.best regards
Please, check the default CRC config and it code produced for STM32F030F4P6 for the v1.11 firmware. It create the errors in EWARM v8.40.2 project (see attach). Revert to v1.10.1 with no problems.Is there hotfix for v1.11?
I have asked this on ST Online Support. I think I should ask it here too.I use System Workbench to 'build all' 2 big packages "as is":STM32Cube_FW_H7_V1.5.0/Projects/STM32H743I-EVAL/ApplicationsSTM32CubeExpansion_SBSFU_V2.2.0/Projects/NUCLEO-H753ZI/ApplicationFor demos that use a HyperTerminal (I use TeraTerm), I don't see the debug printouts to terminal. The TeraTerm setup is pretty straightforward:Connect STM32H753 target with the PC via USB, a STMicroelectronics STLink Virtual COM Port (COMx) (CN23)Open terminal application and connect it via COMx with the following settings: 115200-8-N-1 Is there a switch/jumper on the STM32H753xi EVAL2 Board that I need to change to make this work? I am testing with the following applications:STM32Cube_FW_H7_V1.5.0/Projects/STM32H743I-EVAL/Applications/IAP/IAP_Main (use Serial_PutString())STM32CubeExpansion_SBSFU_V2.2.0/Projects/NUCLEO-H753ZI/Applications/1_Image (use printf())The apps are supposed to print/display a menu on TeraTerm for
I am trying to build and flash sample project from:STM32CubeExpansion_SBSFU_V2.2.0\Projects\NUCLEO-H753ZI\Applications\1_ImageI have been able to build the modules -- SBSFU, SECoreBin and UserApp -- from Makefiles using GNU ARM toolchain.SECoreBin/GNUWARM/prebuild.sh .SECoreBin/makeSBSFU/makeUserApp/makeSECoreBin/GNUWARM/postbuild.sh UserApp/build_debug/UserApp.elf UserApp/build_debug/UserApp.bin 0The last step, postbuild.sh, generated:SECoreBin/Binary/iv.binSECoreBin/Binary/UserApp.sfbSECoreBin/Binary/SBSFU_UserApp.binIt also showed "No FW signing leaf cert" and "No leaf cert" in the output log.To flash:STM32_Programmer_CLI.exe -c port=SWD index=0 reset=HWrst -e all -d SBSFU_UserApp.bin 0x08000000 -HardRstThe app doesn't startup.My question is about the postbuild.sh script that whether the arguments I used were correct. Ultimately I want to bring up the Test Menu from the UserApp.
Hi,I've some problem in understanding why it's not possible to use the single image download on Dual Bank MCU, as "reported" in the following picture (ref. UM2262 pg.54 par. C.2 Mapping Definition).Could someone give me more details about this limitation ? Many thanks,Stefano
I would like to build the SBSFU demo application for the B-L475E-IOT01A on a linux platform, but i can't find any instructions in the documentation or Makefile to do this.
If the Read Protection is set to RDP Level 1 in the Option Bytes, does the above claimed vulnerabilities affect STM32F7xx or STM32H7xx MCUs?
FLASH memory protection is different between STM32G070 and STM32G071.But there is no stm32g070 in the sample project of x-cube-sbsfu package, only stm32g071.Based on project NUCLEO-G071RB, I commented out two protections and compiled them. I wonder if there is any hidden danger in doing so, or if there are any other protections that need to be added?
Hi,We are using STM32F769BIT6 based system for our product. We like to enhance the system with security.Is it possible to add secure boot and encrypted boot to the system without any hardware modification?
Hi everyone,I am using STM32L4A6 with FreeRTOS running on it. I integrate SBSFU according to UM2262 and AN5056. After jumping to application, the firmware triggered Firewall reset when calling osKernelStart() .I already turned SysTick off before jumping to my application. I used one LED to indicate the current code running and firmware was good before calling osKernelStart().I also tried to use non-os application integrated SBSFU and it ran without problem.Any suggestion is welcome. Thanks.Sean
I'm going to play with "Secure User Memory" and RSS feature (explained here) on STM32H753 ,and wonder if it is possible to reset the secure mode using debugger.Of course, unless RDP level 2 is active.Is there a window of time after power-up for a debugger to break in and do full erase of the MCU, or the secure mode will disable debugger interface immediately?-- pa
Hello, I've adapted SBSFU (X-CUBE-SBSFU) example projects for a STM32L4R9 in single bank (flash) mode. I get a firewall reset when accessing SRAM1 that's outside of the defined protected area. Only a small section of SRAM1 is protected by the SBSFU (the secure engine itself, about 4k), so I'm losing quite alot of usable SRAM. According to the STM32L4R errata (en.DM00371862) there are 2 Firewall related limitations: Only 128kB of the 192kB can be protected by the firewall.A 'Spurious' Firewall reset can occur when using FMC or OctoSPI.I'm not using FMC or OctoSPI; I am using LTDC, SDMMC and UARTs.Even when accesing SRAM1 above 128kB (which can't be protected) I get Firewall resets.Using SRAM2 and SRAM3 is ok; no problems there...So following questions:Is the 'spurious' firewall reset possible on SRAM1 above 128kB?Can it be caused by peripherals other dan OctoSPI and FMC?Am I missing something? Any other suggestions?Thank you,rvan
I am trying out the sample projectSTM32CubeExpansion_SBSFU_V2.2.0/Projects/NUCLEO-H753ZI/Applications/1_Image.I have completed the following build steps:prebuild.pyBuild SECoreBinBuild SBSFUBuild UserAppThe last step postbuild.py (which is SECBOOT_ECCDSA_WITH_AES128_CBC_SHA256.sh) has an assert:Exception: AES CBC encryption requires the Firmware Image size (22232 bytes) to be a multiple of the AES block size (16 bytes)I don't know how to get around the problem.
Hi,I am new the the development and I have been testing the hardware aes module.I have tested against a known vector and the results differ from what is expected, I have checked the test vectors using AES provider in .NET and I get the results I expect, so am wondering what is wrong with the code I have.I am running it on a nucleo with the STM32WB55RGV6 MCUThe code is #include "main.h" #define AES_TEXT_SIZE 4 /*TEST VECTORS FROM *https://github.com/ircmaxell/quality-checker/blob/master/tmp/gh_18/PHP-PasswordLib-master/test/Data/Vectors/aes-cbc.test-vectors *Set 3 vector 3 **/ CRYP_HandleTypeDef hcryp1; DMA_HandleTypeDef hdma_aes1_in; DMA_HandleTypeDef hdma_aes1_out; uint32_t aAES256key[8] = {283852128,3195128341,4037964587,2172091781,120337695,3607650619,2735773741,4108260361}; /* Initialization vector */ uint32_t AESIV[4] = {2521758876,2374032254,2071437159, 2100064454}; uint32_t aPlaintextCBC[AES_TEXT_SIZE] = { 1176291376,3001
I have a module that uses the STM32F091RC MCU and trying to connect it with software using C# language.At the first the connection has worked properly, then I've used the CRC32 to verify the sent data but it didn't work.Ive read the "Application note AN4187" and implemented it, I've tried many combinations of CRC32 settings including input data / output data reversion and bit flipping the resulting CRC and nothing matched the results of CRC32 standards when I compared the results using online calculators.Is there any resources that explains the work flow of the hardware CRC32 or how to make it works as standards CRC32?
Hi,I have (for example) a byte array with the size of 6. Now I want to calculate its crc32 value. The first 4 bytes are no problem - I put them in as word, but what about the last 2 bytes?Thanks for the Help in advance.BRNico
Hello,I now understand that I should have asked the question differently.Let's say we have 2 applications: secured and non-secured application.The secured is placed in inetrnal flash, just as done in the demo of SBSFU,But the non secured should be placed in external flash.And we don't need it to be encrypted.Is it that the root bootloader os SB will try to decrypt or authenticate it before jumping to that non secured application in external flash ?The bootloader should decide if jumping to the secured or non-secured according to GPIO (by the way, is it secured ?)Thanksranran
I have a file from ST, not sure where it comes from but the header has:sha1_alt.c for SHA1 HASHCopyright (c) 2017, STMicroelectronicsI am getting issues with the function that call HAL_HASH_SHA1_Accumulate function.They are no checking for size/len if it is 0.For some reason I am getting this issue but not sure if its this file or the application issue.Shall it checks if size is >0 ?Do you have an updated version of this file?
Hi,According to application note for STM32F4xx protection features ,the reverse from RDP L2 to RDP L1 is not possible due to a JTAG fuse, does this mean also that the MCU can check the fuses before checking the RDP? Is it possible to change the Level using UV attack or similar even though the JTAG fuse is blown?Is there any detailed documentation describing how it works to secure FW inside MCU using this feature ?
I'm using the hardware hash processor of an STM32F756 to calculate the MD5 of string "user:realm:password", but the result is wrong. I'm using the HAL library, this is my code.static void AuthRespCalc(char * username, char *realm, char * password) { uint8_t hash[16]; /* HA1 -> HA1=MD5(username:realm:password) */ HASH_Init(); HAL_HASH_MD5_Accumulate(&hhash, (uint8_t *) username, strlen(username)); HAL_HASH_MD5_Accumulate(&hhash, (uint8_t *) ":", 1); HAL_HASH_MD5_Accumulate(&hhash, (uint8_t *) realm, strlen(realm)); HAL_HASH_MD5_Accumulate(&hhash, (uint8_t *) ":", 1); HAL_HASH_MD5_Start(&hhash, (uint8_t *) password, strlen(password), hash, 0xFF); HAL_HASH_DeInit(&hhash); }I'm doing something wrong? Has anyone faced the same problem?Thanks for any help.
..
Dear experts,I'd like to try the Secure Access mode of H753, but overwhelmed by the SBSFU and SFI documentation.I'm thinking about a minimal test for the "secure user memory" - without SFI, Secure Package Creator etc., or as little as possible:Burn a small "blinky"-like test at the start of flash, 0x08000000, in normal unprotected mode, and another small test at the next flash page.Then set the option bytes so that my code at 0x08000000 becomes the secure area, and activate secure mode.After reset, the MCU jumps to my test, in secure mode.My test then jumps to the code in another flash page, exiting the secure mode.All this without any other ST functionality in the system bootloader, and no any crypto stuff yet. The question: can this be done without fiddling with the "Root secure services"? is such a demo available? Thanks in advance, -- pa
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.