Skip to main content
YROSS
Associate
Jun 27, 2019 8:22 AM UTC
Question

RDP level 1 flash protection on STM32H753

Hello,

When the RDP level 1 protection option bytes is set and the boot adress is set in the user flash memory, what are the debugger protections ? Which parts of the microcontroller still remain available via the JTAG debug port or the SWD debug port ?

are the debugger protections the same with a boot adress in system memory (ST embedded bootloader ) ?

Thanks

Yves

This topic has been closed for replies.