Skip to main content
WTom
Associate III
Jun 17, 2019 1:30 PM UTC
Solved

Since the SBSFU doesn't work for all processors, is there a document on how a secure boot process would work with the TPM chip as the root of trust entity?

..

This topic has been closed for replies.
Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
Jun 20, 2019 1:28 PM UTC

Hello,

the next release of SBSFU coming in July will have the ability to connect to ST's STSafe which is a secure element dedicated to IOT.

No TPM interfacing is planned because TPM is overkill for such application.

The SBSFU can be ported on any STM32 processor.

Next release will support other STM32 families such as L0, L1, G4, WB.

F0, F1, F2, and F3 are not supported in the package but a poring could be done

Best regards

Jocelyn

2 replies

Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
Jun 20, 2019 1:28 PM UTC

Hello,

the next release of SBSFU coming in July will have the ability to connect to ST's STSafe which is a secure element dedicated to IOT.

No TPM interfacing is planned because TPM is overkill for such application.

The SBSFU can be ported on any STM32 processor.

Next release will support other STM32 families such as L0, L1, G4, WB.

F0, F1, F2, and F3 are not supported in the package but a poring could be done

Best regards

Jocelyn

WTom
WTomAuthor
Associate III
Jun 21, 2019 1:06 AM UTC

Thanks....looking forward to the next SBSFU release and the new info.