Skip to main content
Vergnani_ElEn
Associate II
Mar 18, 2026 12:26 PM UTC
Solved

How to set FDCAN peripheral in STM32H7 NUCLEO Board

Hi,

I’m trying to configure the FDCAN peripheral on a NUCLEO-STM32H72ZG board, but even though it works perfectly in loopback mode, it doesn’t work when I switch to normal mode. Even in external loopback, when I check with the oscilloscope I don’t see any activity on the TX pin (no signal transitions).

The same issue occurs on this board also with GPIOs.

I tried the same setup on a NUCLEO-STM32F303RE board (using CAN instead of FDCAN), and everything works perfectly there.

 
 

 

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 18, 2026 12:38 PM UTC

Hello,

You said:


@Vergnani_ElEn wrote:

Hi,

I’m trying to configure the FDCAN peripheral on a NUCLEO-STM32H72ZG board, but even though it works perfectly in loopback mode.... Even in external loopback, when I check with the oscilloscope I don’t see any activity on the TX pin


Do you mean that it does work in Internal Loopback mode but it doesn't in External Loopback?

If it works in Internal loopback it should work in External Loopback mode.

For Normal mode you need to establish a complete CAN bus where you are using a transceiver to connect the MCU to the bus and at at least another CAN node that should see your node on that bus to acknowledge the frames sent from your CAN node. This is the minimum hardware requirement to establish a CAN bus:

screenshot.png

CAN is not UART or SPI to monitor the traffic in "open bus" mode.

Related knowledge base articles:

STM32 FDCAN running at 8 Mb/s on NUCLEO boards

How to use FDCAN to create a simple communication with a basic filter

Using CAN (bxCAN) in Normal mode with STM32 microcontrollers (Part 1)

Using CAN (bxCAN) in Normal mode with STM32 microcontrollers (Part 2)

 

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 18, 2026 12:38 PM UTC

Hello,

You said:


@Vergnani_ElEn wrote:

Hi,

I’m trying to configure the FDCAN peripheral on a NUCLEO-STM32H72ZG board, but even though it works perfectly in loopback mode.... Even in external loopback, when I check with the oscilloscope I don’t see any activity on the TX pin


Do you mean that it does work in Internal Loopback mode but it doesn't in External Loopback?

If it works in Internal loopback it should work in External Loopback mode.

For Normal mode you need to establish a complete CAN bus where you are using a transceiver to connect the MCU to the bus and at at least another CAN node that should see your node on that bus to acknowledge the frames sent from your CAN node. This is the minimum hardware requirement to establish a CAN bus:

screenshot.png

CAN is not UART or SPI to monitor the traffic in "open bus" mode.

Related knowledge base articles:

STM32 FDCAN running at 8 Mb/s on NUCLEO boards

How to use FDCAN to create a simple communication with a basic filter

Using CAN (bxCAN) in Normal mode with STM32 microcontrollers (Part 1)

Using CAN (bxCAN) in Normal mode with STM32 microcontrollers (Part 2)

 

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.