Skip to main content

ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

  • 2,813 Topics
  • 11,173 Replies
2813 Topics
ST25R3916B transparent mode configuration problems

前段时间使用ST25R3911B成功实现透明模式的通信,很遗憾的是ST25R3911B不支持负载调制,从而选择ST25R3916B作为替代。目前已经将ST25R3911B透明模式的代码移植到ST25R3916B的芯片上,使用的是OOK的调制方式,移植之后发送数据的已调信号是正常的,接收的信号通过MISO引脚输出异常,如附件图片所示。MOSI引脚负责调制载波,理论上MISO输出的脉宽应该与基带信号一致,这点在ST25R3911B上可以验证。问题1:ST25R3916B在透明模式的接收配置方面,相比ST25R3911B,是否需要更多的配置,避免出现附件里面的问题?问题2:ST25R3916B是否支持在透明模式中,使用负载调制的方式发送数据?Here is the machine translation:Some time ago, ST25R3911B was used to successfully achieve transparent mode communication. Unfortunately, ST25R3911B does not support load modulation, so ST25R3916B is chosen as an alternative.At present, the code of the transparent mode of ST25R3911B has been transplanted to the chip of ST25R3916B, using the modulation mode of OOK. After transplantation, the modulated signal of sending data is normal, while the received signal is abnormally output through the MISO pin, as shown in the attached picture. The MOSI pin is responsible for modulating the carrier, and theoretically the pulse width of the MISO output should be consistent with th