STM32N6570-DK with FSBL and Appl - mapping external PSRAM in FSBL Hello superhero MCU enthusiasts,I'm playing with the STM32N6570-DK and have created a simple project with an FSBL that initializes the MCU and boots the Appl. Once booted, the Appl flashes a "Hello World" LED.Both can be loaded to external flash using the STM32CubeProgrammer.Now, I'm trying to map external PSRAM (XSPI1 -> 0x90000000) inside the FSBL, but it fails.To do that, I change a line in a file in the FSBL, stm32_extmem_conf.h, line 35 of (PSRAM disabled):#define EXTMEM_DRIVER_PSRAM 0Now I try to enable and map the external PSRAM by setting the definition to 1:#define EXTMEM_DRIVER_PSRAM 1However, it doesn't succeed.When debugging I see we land into a HardFault.The FSBL generates a HardFault when executing SAL_XSPI_EnableMapMode, because the function HAL_XSPI_MemoryMapped fails.I can't find the cause.Anyone?I posted a project here with a short Readme.md:https://github.com/AngryCarrot61/STM32N6570-DK_004Note: to see FSBL and Appl working one has to set EXTMEM_DRIVER_PSRAM