Skip to main content
berardo
Associate II
Jul 9, 2013 12:15 PM UTC
Solved

SPC56EL70L5 and SPC56ELADPT144S mini module

Posted on July 09, 2013 at 14:15

Hello,

i have a doubt.

The Daughter/adapter board SPC56ELADPT144S is for SPC56xxEL family.

In SPC56ELADPT144S datasheet is written:  device supported SPC56EL60L5.

But when i search in WEB page for SPC56xxEL family i don't find SPC56EL60L5.

WEB page:

http://www.st.com/web/en/catalog/sense_power/FM2098/SC963/SS1534

in MCU list there are SPC56EL60L3 or SPC56EL70L5.

SPC56ELADPT144S support a MCU that it don't exists?  i think that's impossible!

There is an error?

However, error apart,  are MCU SPC56EL70L5 compatible with SPC56ELADPT144S?

Someone informed?

#spc56el70xx #spc56el70l5
    This topic has been closed for replies.
    berardo
    berardoBest answer
    Associate II
    Jul 11, 2013 10:13 AM UTC
    Posted on July 11, 2013 at 12:13

    Hi,

    thanks for your contribute.

    In addition from ST have confirmed that's ok.

    MCU SP56EL70L5 is perfectly compatible with SPC56ELADPT144S mini module

    2 replies

    Nickname16641_O
    Visitor II
    Jul 10, 2013 7:54 AM UTC
    Posted on July 10, 2013 at 09:54

    Hi,

    The mini module should be compatible with all the EL devices using that socket. It is possible there is an error on the web site, I tested both SPC56EL60 and SPC56EL70 devices in 144pins package.

    Giovanni

    berardo
    berardoAuthorBest answer
    Associate II
    Jul 11, 2013 10:13 AM UTC
    Posted on July 11, 2013 at 12:13

    Hi,

    thanks for your contribute.

    In addition from ST have confirmed that's ok.

    MCU SP56EL70L5 is perfectly compatible with SPC56ELADPT144S mini module