Join discussions in the Product Forums. Ask questions, learn from your peers, and share insights on ST solutions to accelerate your design journey.
Most recent activity
Hi, I'm using the boatd ihmi08. I would like to control the motor in closed loop as a target rotor angle. Is it possible in 6 steps or is the focus much better?
Hi,We have the X-NUCLEO-67W61M1 (for ST67W) attached to a custom STM32U5-board. Disappointingly we just found out the whole architecture of X-CUBE-ST67W61 seems to rely on FreeRTOS while our app architecture is based on ThreadX…A light weight bare metal approach would be highly appreciated when starting up simple testing with e.g AT-commands! Then we want to use ThreadX for an HTTP server among other things.Any recommendations on potential work arounds using the X-CUBE-ST67W61 without switching to FreeRTOS?Thanks in advance
Hello,let say that STM32H753 mCU has connected VBUS (via resistor divider to be sure that voltage on VBUS detection pin (PA9) would never exceed AMR), D-, D+ and GND lines with PC, before mCU core is supplied. At the moment when mCU core is then connected to power supply, would enumeration starts normally as it should or fact that USB module of mCU was connected to PC before core parts of mCU were supplied could bring problems?Thanks!
I'm starting a bare-metal firmware that will display basic graphics on a LTDC connected LCD screen. For the moment I'm using a STM32H53-EVAL2 board (rev E I think) Right now I write a fix image in the frame buffer. The image is correctly displayed except it's kind of blinking. Since the image never changes I suspect it is due to the setup of the LTDC interface or LCD screen. I based my software on STM32CubeH7 source code example (LTDC_Paint application). Do you know: - the screen model on the eval board ( I couldn't find the model in the STM32H753-EVAL2 reference manual) - what configuration parameter could cause the "blinking" of a fixed image ? Thank you
Hello! I'm now using a STM32F469 to drive a screen with MIPI-DSI Interface. I need to send the initial codes with low power command transmission, and then drive the screen in video mode. I think LPDT it is supported by this MCU, but I'm not sure how to use it. Could anyone give me some advice or instructions?
Hello,I am trying to get the OEMiROT example projects running on STM32H563 from "STM32CubeH5\Projects\NUCLEO-H563ZI\Applications\ROT" and this page : https://wiki.st.com/stm32mcu/wiki/Security:How_to_start_with_OEMiRoT_on_STM32H573_and_563%E2%80%93TrustZone_enabled Provisioning works well, unfortunately, I'm blocked on the firmware update step through the internal bootloader. After the message 'Start download with STM32CubeProgrammer through supported interfaces (USART/SPI/I2C/USB)', when I connect CubeProgrammer with uart connection, the bootloader seems to work correctly as I received:Chip ID:0x484 Bootloader protocol version : 4.0Then, CubeProgrammer freezes for 2 mins and the device is disconnected with this message log: 09:54:32 : Error: RDP is set to level 1 or target is held under reset, try using Read UnProtect (-rdu) command in order to remove the Read Out Protection. 09:54:32 : UPLOADING OPTION BYTES DATA ... 09:54:32 : Bank : 0x00 09:54:32 : Address : 0x4
Hello, when I was using this chip, STM32F427ZGT6, it could print data, but the delay was incorrect. After 5 seconds, it was only a few milliseconds. Due to the inaccurate delay, the timing sequence became disordered
I used MC_SDK_6.3.2 to generate a motor control program, but found that sometimes the motherboard crashes. Debugging found that the following code has problems. May I ask why this is? Is it a hardware bug?//The problematic code is here, and the program will enter a dead loop: while (LL_ADC_IsActiveFlag_EOCS(RCM_handle_array[handle]->regADC) == 0u) { /* Nothing to do */ }The complete code is as follows:uint16_t RCM_ExecRegularConv (RegConv_t *regConv) { uint16_t retVal; uint8_t handle = regConv->convHandle; LL_ADC_REG_SetSequencerRanks(RCM_handle_array[handle]->regADC, LL_ADC_REG_RANK_1, __LL_ADC_DECIMAL_NB_TO_CHANNEL(RCM_handle_array[handle]->channel)); (void)LL_ADC_REG_ReadConversionData12L(RCM_handle_array[handle]->regADC); /* Bit banding access equivalent to LL_ADC_REG_StartConversionSWStart */ BB_REG_BIT_SET(&RCM_handle_array[handle]->regADC->CR2, ADC_CR2_SWSTART_Pos); /* Wait until end of regular conversion */ while (LL_ADC_IsActiveFlag_EOCS(
Apologies for cross post, I couldn't find a way to delete the other post or how to change which board to post it to.I'm trying to set up the Utility Sequencer to run an acquisition task followed by an signal processing task, see code snippets below.When I look at the serial monitor, I see the start acquisition task message but then it hangs waiting for EVENT0So even though I've set EVENT0 in Custom_APP_Init() it looks to me that the event is not in fact set.What am I missing here?I commented out the SetTask line as I realized I hadn't finished setting up before the sequencer sets off but now no tasks get set, so I dont get the start acquisition task message any more. #define EVENT0 1<<30 #define EVENT1 1<<31 void Custom_APP_Init(void) { /* USER CODE BEGIN CUSTOM_APP_Init */ UTIL_SEQ_RegTask(1<<CFG_TASK_SENSOR_UPDATE_ID, UTIL_SEQ_RFU, sensor_update); UTIL_SEQ_RegTask(2<<CFG_TASK_FFT_ID, UTIL_SEQ_RFU, do_fft); U
Changelog Version 2.0.0 V2.0.0 implies a breaking change: CMake project generation has been moved from VS Code to STM32CubeMX v6.11.0 (and later). VS Code solution no longer has dependency on STM32CubeIDE (.cproject-files) VS Code solution no longer relies on STM32CubeIDE provided toolchains and debugger tools VS Code solution no longer has dependency on vcpkg, Added support to import STM32CubeMX v6.11.0 CMake projects and bootstrap edit/compile/debug in VS Code Added support to create empty projects Depends on STM32CubeCLT v1.15.0 for empty project creation, build and debug tools Documentation update: The User Guide has increased coverage Better OS platform support https://marketplace.visualstudio.com/items?itemName=stmicroelectronics.stm32-vscode-extension
Hello,I have a small problem here. When I run a clean in git, the directories .vscode, .settings, and build are deleted. If the project needs to be rebuilt, the Setup STM32Cude project function has to be executed manually, and the board/device has to be specified manually again. This is very error-prone. Is there a way to start this project setup from CMake or from CMakePresets.json?For example, if no compiler was found?In CMake, the correct settings are already known.
I've burned a significant amount of time tracking down an issue, so I thought I would share in the hope of helping others and maybe improving ST's provided newlib locks.(This is probably in the wrong place, please move it as required.)I'm using the ThreadSafe files (stm32_lock.h & newlib_lock_glue.c) generated by CubeMX 6.6.1 to make newlib thread safe.I'm utilising Strategy 4: "Allow lock usage from interrupts. Implemented using FreeRTOS locks." (because I'm using FreeRTOS but also the ST USB device library which by default calls malloc from an ISR).Strategy 4 implements newlib's __retarget_lock_etc suite of hooks to lock critical sections inside newlib.To test how robust this solution is I created 3 (exact number not critical, but I had 3 LEDs for debugging...) threads which all repeatedly malloc() and free() in infinite loops.To my dismay it would not be long before a crash/instability occurred.Often the particular "canary" to be killed would be STM32_LOCK_ASSERT_VALID_NESTING_L
Hi. How can I build the Demo FW initially running on NUCLEO-H563ZI ?The is a number of projects in Cube under STM32Cube_FW_H5_V1.5.0\Projects\NUCLEO-H563ZI but it is not clear which one is the factory used to initially program the board. Thanks.
You may encounter an issue when developing for the STM32 microcontroller using STM32 development boards where a pin that is configured for reading on a General Purpose Input/Output (GPIO) reports a high state even when it is not physically connected to any circuit. Pins are not expected to output neither high or low when left floating. This can lead to significant difficulties when developing for the target. In my specific use case, this behavior resulted in an LED flashing when the jumper was not bridged, leading to confusion and misinterpretation of the system's status. It took me more than a week to understand what was happening because debugging step by step using the STMCubeIDE always resulted in the expected functionality. I believe such an issue can arise due to floating inputs and/or electrical noise, mainly if the board is sitting on an isolator.To fix this please make sure to implement pull-up or pull-down resistors in your design to ensure that the GPIO pin h
I've been beating my head for a while trying to use OpenOCD to download my program to the chip, and I'm getting error messages which cite a write algorithm error (errors attached below). I'm not really too sure what I'm doing wrong, and would greatly appreciate any help and insight with resolving this!TL;DR. I'm getting errors likeError: flash write algorithm aborted by target Error: error executing stm32l4 flash write algorithm Error: flash write failed = 00000088 Error: block write failed Error: error writing to flash at address 0x08000000 at offset 0x00000000in the Console log from OpenOCD.I've reproduced the error using OpenOCD with STM32CubeIDE as follows where I set up a fresh project, demonstrate that using ST-LINK (ST-LINK GDB SERVER) works, and finally demonstrate that using OpenOCD fails.I create a new project withFile > New > STM32 ProjectAnd go to "Board Selector", then select the "Commercial Part Number" to NUCLEO-U575ZI-Q.I press "Next >", then fill out the
I'm trying to follow this guidehttps://github.com/jagheterfredrik/meb-preheat I've never used STM32CubeProgrammer or a ST-Link V2 so I don't know what it should look like. I've bought the one at this link https://www.aliexpress.com/item/33010611392.html When I open STM32CubeProgrammer and click "connect" nothing happens, apart from the message in the log windowThe serial number is shown as "E" Do I need to do something to make this device work? Or where can I buy one that works out of the box?
Hi, I am using an STM32N6570-DK running in XIP mode with XSPIM configured in multiplex mode.Setup:XSPIM in multiplex modeXSPI1 / XSPI2 → Port 2 → external flashXSPI3 → Port 1 → PSRAMXSPI2 memory-mapped at 0x70000000FSBL configures external flash and jumps to the application at 0x70100400(VTOR = 0x70100400, MSP = 0x34200000, PC = 0x7010BA01)Everything works correctly in direct XSPIM mode, but in multiplex mode the application HardFaults or hangs immediately after the FSBL jump.The faults occur during early HAL initialization (e.g., in HAL_MspInit() or MX_GPIO_Init()), specifically when executing functions such as: HAL_PWREx_EnableVddIO3();__HAL_RCC_GPIOO_CLK_ENABLE();HAL_RCCEx_PeriphCLKConfig(); If I comment out these lines, the application runs, but then I face issues whenever adding new peripherals (like UART).It seems that reinitializing power domains or clocks related to XSPI pins while executing from external flash triggers a crash. I am using STM32Cube FW
Dear Sir, My board is equipped with STM32G431 MCU. I found that the UART DFU mode of my board does not work after the flash of the MCU has been programmed. The UART DFU mode can only work with a blank MCU that have not been programmed before. I have only used the default setting in the CubeProgrammer. I appreciate if you can give me any suggestion.
Hi all,I am using a nucleo board F412ZG with the Middelware FreeRTOS. I use only one task for now, but I will use others in future.By the way, I set TIM2 as the timer system for FreeTOS:Now I am trying to enable pin PC8 as an external interrupt in order to detect a falling edge: When I generate the code I notice that the TIM2 interrupts is deleted, but I do not understand why. Anyone can help me?Below I leave the screens of the generated code modifies from git:
Hey!I'm trying to run my AI model on my NUCLEO-657X0-Q, following @Julian E. great guide in here.I have 2 questions:1. My model has some running issues during booting.In the FSBL code that suppose to jump to the application (JumpToApplication) there is some crash between the start of __set_MSP() and the start of _set_PRIMASK(), I would say it maybe an error in the pointer to the application code, but when I run it step by step in the IDE's debugger it works just fine.Do you have an idea of why would that happen / how to debug it? (I don't have printings at this stage, and turning in the LEDs in the middle of stack switch makes it fail in the debugger too).2. When my model do run (in the debugger) I get to the point where I start the epoch block, but no outputs / epoch end, and it just gets stuck in the loop. Does it happens because it's in debugger mode, or maybe my model is not compatible? when I validated it in CubeMX AI extension it looked ok.Is there any way to debug
Hi all,I'm trying to use Livetune to make an mp3 player but it only works once connected to a board. I have a custom Nucleo-U5A9 (originally a Nucleo-U575, I replaced the MCU and added xtal). I'm reading UM3297 Getting started with X-CUBE-AUDIO-KIT and on page 6 (picture below) says:"The connection is successful only if the firmware running on the device includes the Designer communication firmware."I would like to include this "Designer communication firmware" into my custom board/firmware but I can't seem to find any reference to it anywhere. I'm pretty sure is part of the examples firmware but I rather not hunt for it that way unless there is an example for the U5A9 which I don't see. Even so ... this "Designer communication firmware" doesn't seem to be designated as such in the example projects.where is this "Designer communication firmware"? How do I integrate it into my custom U5A9 board?Any help is appreciated... thanks.
Hello,I moved an existing project from 1.14 to 2.0.0. To be clear I created a new workspace, then a new project in 2.0.0 in order to prevent any non relevant bit taken from 1.14 (at the project level) and copied only the source files from 1.14 to 2.0.0. The linker file comes from 2.0.0, as well as the startup file (which is not relevant here).When I compile I get the error that elf has LOAD segment with RWX permissions. The linker file has the READONLY moniker where they are needed, but I have 3 functions that are running from RAM, with __attribute__ ((section(".RamFunc"))). Obviously these are executables, so it is expected to have RWX in the .data section, where .RamFunc resides.How can I get rid of this warning, please ?Even though it is not relevant, the MCU is an STM32G0B1CB.
Post edited by ST moderator to be inline with the community rules for the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code. Hi,I want to jump to system memory boot with SW using UART1.I tested it using code I found by searching forums and the internet, but it doesn't work.For reference, the STM32G071 shares the BOOT0 and SWCLK pins. By pulling the BOOT0 pin high and resetting the device, I can perform a system memory boot. After that, I connected the UART connect in STM32CubeProgrammer and verified the update. However, after jumping to the code below and pressing the UART connect in STM32CubeProgrammer, the following message appears and the device fails. RTS lowDTR lowSerial Port COM15 is successfully opened.Port configuration: parity = even, baudrate = 115200, data-bit=8, stop-bit=1.0, flow-control=0ffTimeout error occurred while waiting for acknowledgment.Error: Activating device: KO. Please verify the boot mo
Hello. I'm trying to get the LVGL library running on the STM32H7S78. The simple DMA2D variant (LV_USE_DRAW_DMA2D) with 16-bit color depth works perfectly, but it's not very performant. Therefore, I'm trying to get the LV_USE_NEMA_GFX variant running instead. The basis is LVGL version V9.3, which already runs on an STM32U5 with NEMA_GFX. However, the problem is that it always crashes during initialization in lv_draw_nema_gfx_init(). lv_draw_nema_gfx_unit_t * draw_nema_gfx_unit = lv_draw_create_unit(sizeof(lv_draw_nema_gfx_unit_t)); /*Initiallize NemaGFX*/ nema_init(); draw_nema_gfx_unit->base_unit.dispatch_cb = nema_gfx_dispatch; draw_nema_gfx_unit->base_unit.evaluate_cb = nema_gfx_evaluate; draw_nema_gfx_unit->base_unit.delete_cb = nema_gfx_delete; draw_nema_gfx_unit->base_unit.name = "NEMA_GFX"; /*Create GPU Command List*/ draw_nema_gfx_unit->cl = nema_cl_create(); /*Bind Command List*/ nema_cl_bind_circular(&(draw_nema_gfx_unit->cl));
Hello,I am currently designing a custom PCB with the STM32WLE5CC (QFN package) targeting +22 dBm in the 868 MHz frequency band.I have been following the reference design based on the MB1720 board, which is specifically described as being for +22 dBm at 868 MHz. However, I don’t fully understand why, in this high-power configuration, the solder bridge for RFO_LP is closed while RFO_HP is left open.Could you please clarify the reason for this choice in the reference design?Thank you in advance.
ST Community highlights – April to June 2026
Already have an account? Login
No account yet? Create an account
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.