Skip to main content
Associate II
Dec 9, 2025 4:26 PM UTC
Question

STM32U073CCT6 - STOP MODE 2 Power Consumption

Hi

 

We are using an STM32U073CCT6 on a battery-powered board. We need to put the processor in low-power mode to increase battery life. The current in STOP MODE 2 is about 20uA. To address some issue related to the power supply and our hardware, we put the processor in Shutdown Mode and obtained a current of 2uA. How could we reduce the consumption in STOP2 mode? We have already deinitialized all peripherals before entering stop mode 2.  

 

BR

Gilberto

5 replies

MM..1
Super User
Dec 9, 2025 6:42 PM UTC

695 nA without RTC

primary check if isnt wake periodic

Associate II
Dec 9, 2025 7:05 PM UTC

Hi

It is not for sure. It use the RTC for wake up 30 seconds. I have managed to get some further reduction in power consuption placing the GPIO in analog mode. 

Is there a clock that I need to manually disable?

 

BR

Gilberto

Gyessine
ST Technical Moderator
Dec 10, 2025 8:21 AM UTC

hello @gilberto-falker 
Based on the product datasheet, it is possible to save additional µA. A consumption of 20 µA is still significant for Stop2 mode.
Did you review this article? It may provide useful insights.
However, if you still need to reduce power consumption after applying the tips from the article, consider refining your hardware.
Hope taht helps
Gyessine

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate II
Dec 10, 2025 2:08 PM UTC

Hi

Thank you very much! Excellent publication!
Regarding the HAL_PWR_EnableSleepOnExit() function:

Is there any way to ensure that the processor does not enter stop mode when receiving an int between the two function calls below:

HAL_PWR_EnableSleepOnExit();

HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);

BR

Gilberto

Gyessine
ST Technical Moderator
Dec 11, 2025 8:43 AM UTC

hello @gilberto-falker 
well,the

HAL_PWR_EnableSleepOnExit()

is designed to make the processor re-enters SLEEP mode when an interruption handling is over.
if you don't want your processor to enter stop mode when receiving an interrupt between your two functions
you can use

HAL_PWR_DisableSleepOnExit();

to prevent this from happening, maybe you can try this implementation .

HAL_PWR_EnableSleepOnExit();
HAL_PWR_DisableSleepOnExit();
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);

In general, you can control it manually by disabling sleep on exit when you don't need it.
Hope I understood and answered your case correctly.
Gyessine.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.