Skip to main content
Visitor II
Dec 11, 2025 2:28 AM UTC
Question

SRAM3 memory block availability for STM32H742xI/G

Hi,

In STM32H742xI/G datasheet (DS12110 Rev 8), the SRAM3 memory block is not specified in the "Table 7. Flash memory and SRAM memory mapping" but I can see the availability of the SRAM3 in the generated .map file.

Can someone please confirm, it is typo mistake in datasheet or really not available for STM32H742xI/G?

palanib_0-1765419963955.png

palanib_1-1765420104807.png

 

Thanks

1 reply

ST Technical Moderator
Dec 11, 2025 9:03 AM UTC

Hello @palanib and welcome to the Community

After deep check, the datasheet is correct as the SRAM3 is not available in STM32H742x devices.

This is mentioned in the Table 2. STM32H742xI/G and STM32H743xI/G features and peripheral counts in the DS12110 Rev 10 and with more details in the AN4891 - Table 6:

ImenD_0-1765443276858.png

Please provide more details on your project to better understand and reproduce your case:

Which project are you using? 

which version of Cube package and tools used? 

How did you generate your project and the map file? 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks