WATCH ON-DEMAND | STM32 Summit 2026
Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.
Most recent activity
Posted on February 10, 2016 at 16:24Hi,Now I am sending AT Commands in two ways1. through Tera Term 2. through UART ( Wifi Module Connected to my MCU via UART )Is there any other way to send AT commands ?Is it possible to send AT commands on air ???
Posted on October 05, 2015 at 02:38I'm wanting to load a custom firmware onto the SP1ML-915, as I'd like to implement abilities I can't get through the existing AT command set. Where can I find documentation about how the STM32L151RB is connected to the Spirit1 chip? i.e. which spi on what pins? Also, does STM32CubeMX offer any help in setting up a base for a this type of firmware? Would appreciate any pointers, as I'm fairly new to all of this.
Posted on February 04, 2016 at 17:03Hi all, I have a problem. I use Wifi module in miniAP mode. I started to listen UDP socket in port 18120 and connect one client to this socket and go to data mode. When i send data from client to wifi module and next to MCU everything it is ok. But In most case when i send data from MCU to client over wifi module, data lost. I think this is problem of FW in module. I check uart data in scope and it is ok, MCU send data to wifi module. Anybody have same issue? Thanks for help, Ondra FW version: 141106-0950875-SPWF02S ( i think this is v3.3)
Posted on February 19, 2015 at 09:42HelloI have 2 STEVAL-SPBT3ATV3 to evaluate an application and the first BlueModule is on v1.6 for the firmware and the 2nd is on v1.3.How i can find and download the FW v1.6 for upgrade ?Thanks for your respond #bluettooth-spbt2632c2a.at2
Posted on January 20, 2016 at 07:51Good Morning, I tried the FirstSet function and it worked fine without special characters. I tried it also with percentage encoding, but it doesn't work, like expected. The FirstSet function is a good way to configure a device with limited user input possibilites. But it is mandatory to use special characters for the password. So, is it planed to add some encoding (e.g. percentage encoding'') to the FirstSet function, so that I can use this function for networks with passwords with special characters? Cheers, Flow
Posted on January 29, 2016 at 14:05When I configure one module to listen on a port I can then connect to it via PC client and enter data mode. At this point a link is established and communications are asynchronous bidirectional. When configuring one module to listen (same as above) and another to connect to a port (AT+S.SOCKON=<ip>,<port>,u), the connection can be made but data mode (AT+S) cannot be enabled on either device and communications are not bidirectional like it was talking to pc. Am I missing something obvious here? Whats the difference between talking UDP to a PC client or the module client?
Posted on January 27, 2016 at 09:02Hi all, I have software circullar buffer, parser, state machine for wifi module SPWF01. Everything is ok, but i must loaded data in IRQ every one byte. I will used DMA circle buffer and loaded long data burst but i think this is not possible, because module had not define rules for comunication frame length. Please tell me im wrong and communication frame lenght has define frame lenght (long as 2^n byte or some others rule). Thanks for reply. Ondra
Posted on January 29, 2016 at 12:17Hello, Please help to clarify the following: Can I use BlueNRG-MS module in slave and broadcast mode simultaneously? So, I would like to have connection with master and send some broadcast message. Thanks in advance Regards, Andrei Kukenov
Posted on January 26, 2016 at 19:54Hello.Why when I use sending of ACL packet it is take to 4-8 second for acknowledge event?How can I setup this duration?Which type of ACL packet does BlueNRG use?( DM1, DH1, DM3,DH3, DM5, DH5 and AUX1. 2-DH1, 3-DH1, 2-DH3, 3-DH3, 2-DH5 and 3-DH5.) #bluenrq #event #acl
Posted on January 25, 2016 at 16:37 Hello, I have bought 2 SPSGRF-868-Nucleo module. I want for beginning sent a packet for see how spirit1 works. But afters some search, I don't know if my packet is really sent or not because I receive anything. I have configured 1 module for do a TX and other for RX. TX seems work, because when I sent a packet the interrupt for TX data sent is SET. For RX, I have no interrupt request for RX data available. Only discard. This discard says that the RX timeout is done. I have configured my module with this parameter : // To define : #define XTAL_FREQUENCY 50e6 #define FREQUENCY_OFFSET 0 #define POWER_DBM 6 /* SRadioInit struct */ #define XTAL_OFFSET_PPM 0 #ifndef IF_DEF_RX #define BASE_FREQUENCY 868000000 #else #define BASE_FREQUENCY 868480000 #endif #define CHANNEL_SPACE 20e3 #define CHANNEL_NUMBER 0 #define MODULATION_SELECT FSK #define DATARATE 38400 #define FREQ_DEVIATION 20 #define BANDWIDTH 5e3 /* PktbasicInit struct
Posted on January 15, 2016 at 17:30Hello. Could you tell how IRQ is work? Does setup automatically after command write to BlueNRG over HCI? #bluenrg #spi #hci
Posted on January 21, 2016 at 13:33Hi everyone, I'm making a comparison of different SoM for IoT. I found the SPWF01SA which matchs with my needs. But I want to know the heat generated by this module. Does someone have this data ?
Posted on January 22, 2016 at 10:02Hi!I have connected my Wi-Fi module with a client and now I am getting the commands+WIND:61: Incoming Socket Client :172.31.142.2+WIND:60: Now in Data Modenow I want to get back to command mode.I have tried hitting escape button , Also I tried sending AT+S. without <CR><LF> it is not working. How can i get back to command mode ?Also they suggest to send escape sequence(how can i send escape sequence ?)
Posted on January 09, 2015 at 18:46Hi, I'm trying to customize the advertising packet, but it's unsuccessful so far. I use STEVAL-IDB002V1 BlueNRG HW v3.0BlueNRG FW v6.4Motherboard FW v1.4Since the command ACI_GAP_SET_DISCOVARABLE doesn't give much options I've tried to use HCI_LE_SET_ADVERTISING_PARAMETERS , HCI_LE_Set_Advertizing_Data, HCI_LE_SET_ADVERTISE_ENABLE. The response to HCI_LE_SET_ADVERTISING_PARAMETERS and HCI_LE_SET_ADVERTISE_ENABLE is Unknown HCI Command.Are these supported commands?Is there any other way to customize the advertising and scan packet?Thanks
Posted on January 20, 2016 at 16:08Hello all,I'm using a SPWF01SA.11 as a web server. It is coupled with an host MCU that process the http protocol: the internal web server on the module is disabled (ip_use_httpd = 0), and I have opened the socket server on port 80 (AT+S.SOCKD = 80,t). In this way when the mcu receive an http request, it reply with the http header and the content of the html page. To load a page, the mcu sends over the uart a block of 800 bytes of data and waits for ip_sockd_timeout + 45ms before sending another block. This delay is intended to allow the sending of the data over the wireless and avoid the buffer overflow. Ip_sockd_timeout is set to 5ms. With this configuration sometimes I have some tcp packets corrupted (filled with zero) and the html page is not loaded. Unfortunatelly I can't use hardware flow control because I have some hardware constrains. Is there a solution to safely send some kB of data without having data loss?Thanks in advance for the support.
Posted on January 20, 2016 at 08:54Hello all,we need the test report about the ETSI EN 300 328 certification in order to proceed with the certification of our final product. Thank you,Marco
Posted on October 27, 2015 at 15:40Hi,I would like to communicate with the LCD display. How can i connect the display?. Are there any separate pins dedicated for LCD data bits or i can connect to any GPIO pin. Here i would like to send the serial data (SPI) of a 3-axis sensor to LCD display.
Posted on January 17, 2016 at 19:07Hi (Gerry), if I download a file via HTTPGET command, the content of the file is changed by the wifi module. The file contains 0x00 data. The wifi module translates this into 0x20. Can anybody tell me how to fix this? Thx & cheers, Flow
Posted on December 04, 2015 at 10:11Hi, I have the STM32F411 Nucleo with X-NUCLEO-IDB04A1 BLE expansion module.I attempted to download the X-CUBE-BLE1 expansion software from the link below, but no ''download'' button available. http://www.st.com/st-web-ui/active/en/catalog/tools/FM146/CL2179/FM147/SC1870/PF261442 Any ideas to get this module and integrate it to STM32CubeF4 ? Thanks
Posted on January 13, 2016 at 13:34Hi , BlueNRG_Stack_IFR_Updater What is the use of above application which is available in the '' \BlueNRG DK 1.8.0\Projects\Projects_Cube '' -- Regards Ratheesh T
Posted on February 03, 2015 at 08:49Hi everyone, I was wondering if there is an updated version for the UM1755 which (partially) describes the commands available for the BlueNRG chipset. I can't find decoding scheme for the VS HCI events for example.Thank you.
Posted on January 10, 2016 at 18:37Hi,I'm interface the BlueNRG directly (not using the ACI stack), and having problems programming a Central device when trying to configure scan parameters. Here it is my sequence of events and commands:1) 04 FF 03 01 00 01, BlueNRG ready after reset 2) 01 0C FC 08 00 06 BB 00 00 E1 80 02, Write config. data (BT address) 04 0E 04 01 0C FC 00, Command complete 3) 01 01 FD 00, GATT init 04 0E 04 01 01 FD 00, Command complete 4) 01 8A FC 01 03, GAP init (Role = Central) 04 0E 0A 01 8A FC 00 05 00 06 00 08 00, Command complete & handlers 5) 01 0B 20 07 00 40 00 40 00 00 00, LE Set Scan Parameters (passive scan, interv, wnd) 04 0F 04 01 01 01 0B 20, HCI command unknown (ERROR)I've tried also other LE related commands like LE_Set_Scan_Enable (200C) without success.I don't want to use instead any discovery procedure that will trigger active scanning. I just want the easiest way t
Posted on January 08, 2015 at 00:10Hello - I have run 4 different boards, X-NUCLEO-IDB04A1, from the debugger, stopping on a break point right after a call to hci_read_bd_addr() (which returns success), and all 4 boards had this same board address: 04:02:EC:25:00:FD In order to go into commercial production with a BTLE product, is it required to ensure unique board addresses? In other words, is it required to buy a block of addresses and ensure that each board produced uses exactly one of the block bought? Thanks, #ble-ieee-board-address
Posted on December 09, 2015 at 16:55How do I set a true random address? Using hci_le_set_random_address() I get 0xFF FF FF FF FF FF. Hardware is Nucleo-L053R8 & IDB05A1 Also setting a Beacon with BlueNRG GUI v1.8.0 with a random address also results in a address of 0xFF * 6 Following is the code I tried:- uint8_t RANDOM_BDADDR[] = {0x55, 0xaa, 0x55, 0xaa, 0x55, 0xaa};uint8_t bdaddr[BDADDR_SIZE];uint8_t stack_mode = 4;BlueNRG_RST();ret = aci_hal_write_config_data(CONFIG_DATA_ROLE,CONFIG_DATA_ROLE_LEN,stack_mode);ret = hci_le_set_random_address(RANDOM_BDADDR));ret = hci_read_bd_addr(bdaddr);// bdaddr = 0xFF FF FF FF FF FF !?!
Posted on January 08, 2016 at 16:55Hi, I would like to know if BLUENRG MS supports ANT protocol ?
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.