Skip to main content
T.Ratheesh
Associate II
Feb 4, 2016 12:55 PM UTC
Question

BlueNRG TX & RX Buffer size Restriction ?

Posted on February 04, 2016 at 13:55

Hi all,

          In BlueNRG chat application, i can able to transfer and receive data if  the packet size was 20 or below. When i change the packet size more than 20 bytes , communication doesn't started. But i need to transfer 35 bytes at a time.

Where i have to change packet size?

Thanks in Advance

Regards

Ratheesh
This topic has been closed for replies.

1 reply

marchese.graziella
Visitor II
Mar 9, 2016 2:54 PM UTC
Posted on March 09, 2016 at 15:54

Dear Customer,

the BlueNRG chat application is based on Notification, in fact the slave will continuously send notification of 20 bytes to the client and the notification are of 20 bytes.

To transfer more than 20 bytes, you cannot use the notification.

Regards,

GM