Skip to main content
jgarr
Associate
Jan 29, 2016 1:05 PM UTC
Question

SPWF01SA UDP Connection Inconsistent

Posted on January 29, 2016 at 14:05

When I configure one module to listen on a port I can then connect to it via PC client and enter data mode. At this point a link is established and communications are asynchronous bidirectional.

When configuring one module to listen (same as above) and another to connect to a port (AT+S.SOCKON=<ip>,<port>,u), the connection can be made but data mode (AT+S) cannot be enabled on either device and communications are not bidirectional like it was talking to pc. Am I missing something obvious here? Whats the difference between talking UDP to a PC client or the module client?
    This topic has been closed for replies.

    4 replies

    Gerardo GALLUCCI
    ST Employee
    Jan 29, 2016 1:48 PM UTC
    Posted on January 29, 2016 at 14:48

    Hi Jason,

    CommandMode/DataMode exists only on socket server (SOCKD). Socket client are always in CommandMode.

    Check ''Data Mode'' on forum main page. There are a lot of threads on how to use CM/DM.

    Regards

    j

    jgarr
    jgarrAuthor
    Associate
    Jan 29, 2016 7:42 PM UTC
    Posted on January 29, 2016 at 20:42

    Thanks, that clears things up.

    Now after doing some testing I'm finding that this operation inherently makes the module asymmetric in that it can receive many more packets/s than it can send (5byte payload). I can Rx > 160/s with minimal loss but Tx i begin to get hard faults as soon as i get below 20/s. Is there a trick here or is it just the nature of the beast?

    Gerardo GALLUCCI
    ST Employee
    Jan 29, 2016 7:46 PM UTC
    Posted on January 29, 2016 at 20:46

    Which FW version are you using? I don't expect hardfaults using latest version.

    Please update. Contact your local distributor.

    Thanks

    j

    jgarr
    jgarrAuthor
    Associate
    Feb 1, 2016 3:39 PM UTC
    Posted on February 01, 2016 at 16:39

    V3.4