WATCH ON-DEMAND | STM32 Summit 2026
Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.
Most recent activity
Posted on December 05, 2016 at 21:13shield of stm32f746g discoveryshield of the idb04a1is there a solution (difficult to unsolder the resistance: can we curve or cut the pin and stripe irq csn and clk ?)Br,Christophe#bluenrg #stm32f746g-disco
Posted on December 06, 2016 at 15:28Hi,I'm using the Bluenrg-ms chipset with firmware version 7.1.e (0x715). Everything works fine, except from the authorization settings. Each device can connect to the BLE without any request for permissions (PIN). By digging a bit I've found that the function 'aci_gap_slave_security_request' should do the job, but I don't exactly know where and how to use it (related callbacks to handle, actions to do according to the result). Can anybody help me through this?Thanks a lot,Daniele#spbtle-rf #bluenrg-ms #ble
Posted on May 30, 2016 at 07:10I have our BlueNRG device set up to use a fixed pin for pairing. I am able to successfully pair with Apple iOS decvices and windows phone when I enter the correct PIN when prompted by the device. However when connecting to an Android device, the pairing always fails even though I enter the correct PIN when prompted. Using a packet sniffer I can see that the reason for failing is 0x04 (The confirm value does not match the calculated compare value). I have tried with several different Android devices and versions including 4.4, 5.1 & 6.0 and I have the same issue with all of these. Has anyone successfully paired an Android device with BlueNRG using a PIN code? Regards Nick #bluenrg-pairing #android #android #bluenrg-pairing
Posted on November 24, 2016 at 11:26Hello, I am using SPWF01.11 FW3.5 as webserver as described in a previous post. This webserver is made of 1 HTML Frameset (main.html) + 3 HTML frames (m.html / sm.html / data.html) to override the 4ko limitation. I am also using local jQuery (v 1.2.3) (53Ko). My static pages are created with httpd_gen.exe creating outfile.img. This webserver work well on my desktop PC + several smartphone using android or iOS 8.4. I then try on different iphone with iOS 10 and the pages are blocked (I tested Safari/Firefox/Opera Mini with all the same problem). Consulting safari error consol I get the message: ''Sandboxing m.html beacause it is using HTTP/0.9'' ''Stopped document load from m.html beacause it is using HTTP/0.9 on a non default port'' The 3 HTML frames pages have the same problem. The problem of non-default port is strange as my server is tested on port 80. As I don't know much about HTTP version, my questions are: - does anyone enc
Posted on November 23, 2016 at 15:58Hi, how can I configure/deactivate the Nagle-Algorithm in SPWF01S? Thanks! MBU
Posted on November 21, 2016 at 20:59Hello everyone!I'm working with ST SPBLE-RF using the C code driver provided for BlueNRG-MS. I ported it for an ST8L151G6 microcontroller; the SPI communication works, the device answers correctly (0x02 and the R/W buffer sizes), it pulls up the IRQ pin etc. It sends the vendor specific event (0x04FF03010001) indicating it is initialized. My problem is with all the other commands; i tried (following the examples in the stack) to set the MAC address with the API, but it always return an error, not a timeout but instead of a 'command complete' event i receive a 'command status' with the data 0x040F0101FC0C. The code (inside the hci_send_req API) checks the returned data (in the SPI_IRQ ISR) but it stops because it checks for r->event (always set to 0) and then the third byte (01) of the received data, that it is not null and so it fails. The same problem is found with every command (set TX power, read configuration etc)What is the problem? someone
Posted on November 18, 2016 at 23:27Hi, i have a problem using SensorDemo_New of BlueNRG DK 2.0.2COPY_ENV_SENS_SERVICE_UUID(uuid); ret = aci_gatt_add_serv(UUID_TYPE_128, uuid, PRIMARY_SERVICE, 10, &envSensServHandle);i get ERR_UNSPECIFIED_ERRORif change max_attr_records to 7: ret = aci_gatt_add_serv(UUID_TYPE_128, uuid, PRIMARY_SERVICE, 7, &envSensServHandle);i get ERR_UNSPECIFIED_ERROR when call: /* Humidity Characteristic */ if(sensor_board){ COPY_HUMIDITY_CHAR_UUID(uuid); ret = aci_gatt_add_char(envSensServHandle, UUID_TYPE_128, uuid, 2, CHAR_PROP_READ, ATTR_PERMISSION_NONE, GATT_NOTIFY_READ_REQ_AND_WAIT_FOR_APPL_RESP, 16, 0, &humidityCharHandle);Any suggest? Regards, D.#####################################################
Posted on November 15, 2016 at 08:58Hi..I can easily connect the module to any APs and it works fine. But, I can not connect it to the iPhone hotpots.. does hotshots needs additional configuration.?
Posted on November 18, 2016 at 12:18I have been using the your WiFi module, The module desciption is below; # nv_manuf = ST # nv_model = SPWF01SA1 # nv_serial = 4313D02202 # nv_wifi_macaddr = 00:80:E1:FF:BA:10 +WIND:1:Poweron (141106-0950875-SPWF01S) (f/w version) After socket write operation with''AT+S.SOCKR'' command, ''+WIND:55:Pending Data...'' is generated. UM1695 does not include any information about that issue. I upgrate the firmware from 3.3(141106) to 3.5(160129) I retest the module but got same result. I attached the test outputs screen shot. I already test two modules but the result is same.
Posted on November 15, 2016 at 17:10Hi,I'm trying to send messages to the host processor (the one communicating with the SPWF01SA module).As far as I know there are two methods:* /output.cgi?text=message* SOCKDBoth output.cgi and the socket server suffer from the fact that messages are indistinguishable from asynchronous indications from the SPWF01SA module.If I were to send two requests to output.cgi:/output.cgi?text=/output.cgi?text=+WIND:2:ResetThe host processor would now think that it received a valid WIND. The first request to output.cgi sends ''\r\n'' and the second ''+WIND:2:Reset\r\n'' resulting in ''\r\n+WIND:2:Reset\r\n'' which is identical to a WIND.We have this same issue when a socket client connects to the socket server. Even when we are in Data Mode, we must continuously monitor WINDs for returning to Command Mode.In this case the socket client can simply send: ''\r\n+WIND:59:Back to Command Mode\r\n\r\n+WIND:2:Reset\r\n'' which will have the same effect as the output.
Posted on October 21, 2016 at 14:55Hi, I'm trying for lowest bandwidth settings for higher sensitivity. But packets wouldn't reach. Is there any problem with my settings? #define CHANNEL_SPACE 20e3 #define CHANNEL_NUMBER 0 #define MODULATION_SELECT FSK #define DATARATE 1200 #define FREQ_DEVIATION 1e3 #define BANDWIDTH 6E3 #define POWER_DBM 11.6 #define POWER
Posted on November 10, 2016 at 12:03Does anyone know if ST have source code for the SP1ML modules available? or even a starting point for people wanting to develop custom firmware for the device.thanks #sp1ml-spirit1-stm32l151rb
Posted on November 02, 2016 at 21:32I'm trying to add a ''Client configuration descriptor'' to a characteristic using the following function call. However, it returns a status of 0x61 (invalid parameter) with no indication of which parameter is invalid. This call DOES WORK for all valid descriptors except for ''CHAR_CLIENT_CONFIG_DESC_UUID'' and ''CHAR_SERVER_CONFIG_DESC_UUID''. Anybody have any idea which parameter my be wrong?--------------------------------------------------------------------uuid16 = CHAR_CLIENT_CONFIG_DESC_UUID;uint16_t descHandle;charactFormat charFormat;charFormat.format = FORMAT_UTF8S;charFormat.exp = 0;charFormat.unit = UNIT_UNITLESS;charFormat.name_space = 0;charFormat.desc = 0; status = aci_gatt_add_char_desc(service_handle, characteristic_handle, UUID_TYPE_16, uuid16, 7, 7, (void *)&charFormat, ATTR_PERMISSION_NONE, ATTR_ACCESS_READ_ONLY | ATTR_ACCESS_READ_WRITE, 01, 16, FALSE, &
Posted on November 02, 2016 at 18:23Hi,I've been testing the socket server (AT+S.SOCKD=32000) on the SPWF01SA and noticed that whenever a client connects the Wi-Fi module immediately enters data mode. This seemed like a potential problem so I decided to test it while waiting for the result from an AT command (HTTPGET).Interestingly, the message from the socket client is printed immediately on the UART (no WIND!) and the AT command does not complete until the socket client disconnects. After the socket client disconnects the response from the AT command is printed followed by four WINDs (61, 60, 59, 62).This behaviour makes it dangerous to have a socket server active while issuing any AT command.If a socket client has connected previously, I am able to enter and exit data mode (at+s.) with success. If there is incoming socket data during this time I properly get WIND 64 (pending data) and am able to receive it later (with at+s.).Example to reproduce (UI = UART Input, UO = UART Output,
Posted on October 28, 2016 at 01:38HelloI'm evaluating the SPWF01SA for an industrial application especially with regard to its TLS capabilities.Unfortunately my knowledge of TLS especially in an embedded setting is limited, and AN4683 neglects to mention how the SPWF01xx module handles a few key aspects of TLS which I think are important to understand. Specifically,Is there any check for revoked certificates?AN4683 mentions the server certificate is verified, but how are certificate chains processed? My understanding is that every certificate in the chain should be verified. Does the SPWF01xx do this when provided the top-most root CA certificate, but is connecting to a server several certificates down the chain?Are there any other drawbacks or considerations worth noting? Regards, m
Posted on October 19, 2016 at 15:46Hi,I am doing some measurements using the RSSI from the SPIRIT1. I am making the the following test:In the transmiter I am using the continuos wave In the receiver I am verifing the RSSI as the following:Enter RX state,Waiting some us (~180)SABORT CommandReading de Register 0xC8With a distance of 10m between transmiter and receiver I can see the RSSI in the receiver going lower when the transmiter power goes low, GREAT!The problem is when I am using the transmiter to send packets. Does not matter if I change the power transmited from 16dBm to -30 dBm. In the receiver my RSSI measured is always -54 dBm, using the same distance from the test with a transmiter in continuos wave.I know that the power in the transmiter is changing, because I am using a spectrum analyzer to check it.I would like to know if anyone has some insights about what could be happening. I am looking at the registers related to the RSSI, like RSSI_FLT. I do not understand how t
Posted on July 28, 2016 at 12:59Hi, I am a beginner with RF and SPIRIT1. I’ve been working with SPIRTI1 for more than a month by now and I am having some problems regarding de cofiguration of the output power of this device. I am not able to get +16dBm as output power from the CI I am using. I used a spectrum analyser to measure the frequency and output power of the SPIRIT1 and as result I got -1.95 dBm as output power, the parameters refering to frequency are correct, but the output power is much lower of what I was expecting. I would like to ask for some ideas of what could be wrong with my design (hardware and/or firmware).The SPIRIT1 is working at 172MHz, GFSK with BT = 1, basic packet, 100kbps data rate, output power = +16dBm (at least, it should be).I am able to transmit and receive basic packets up to a distance of 50m without any erros, using CSMA or not, with CRC filtering enable.Regarding the output power, do I only need to set those two registers? POWER[8] (0x10) and POWER[
Posted on October 13, 2016 at 21:18Hi guys,SPWF01S is a new module for me. I have been using it for about a month.My question is this: if I set the WiFi connection options at every boot and issue an AT&W (save), will it wear out the eprom memory? How do you guys handle configuring the module at boot?Due to legacy design I am not using an ST processor :(-Mr_E #wifi
Posted on October 18, 2016 at 14:17Hi, UM1695 mentions that there is a special test mode that is enabled via configuration variable ''eft_mode''. Description says ''Enable/disable the Engineering Test Functions. It is used for controlling the radio for the certification tests (disabled by default=0, enabled=1)''. However I cannot find any more documentation on this. Typically in these tests we would like to select the channel and transmission and jut send some data patterns in order to measure the antenna implementation etc. How are these controlled when test mode is enabled?
Posted on September 19, 2016 at 22:07Hello everyone, the documentation about the AT+S.HTTPREQ is very limited. I would like to download quite large files from an HTTP server. I've been told that it is possible to request small parts of the file with a curl -r command. Is it possible to do such a thing with the AT+S.HTTPREQ command or any other way. Thank you. #at+s.httpreq
Posted on October 03, 2016 at 13:49Dear all,I have already posted /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/Where%20to%20find%20a%20programming%20manual&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&currentviews=53, they suggest me to post in this other subforum.So, I am trying to find a programming manual or a reference manual for SPBTLE-RF on the st website without success. I have found only a datasheet but nothing else.I am looking for this programming manual since it seems this chip is used on the newest bluetooth x-Nucleo and I am working on a project which aims to support every or the most part of STM32 expansion boards, but this is becoming more and more difficult. Hints?Ciao,RM null
Posted on October 14, 2016 at 23:55I have a server socket that automatically goes into data mode when a client connects.I would like to be able to go back to command mode by using the escape sequence ''at+s.'', but it doesn't work, even if I set a custom escape sequence.♯ nv_manuf = ST♯ nv_model = SPWF01SA1♯ version = 160129-c5bf5ce-SPWF01SSpecifically: the client sends me new WIFI config info. SSID, etc. I'd like to read each item, have the main processor set that option on the WiFi module, then echo back the reply to the client. I know I can read data on a socket while in command mode. The question is will a server socket allow command mode? #command-mode
Posted on October 06, 2016 at 11:35We are testing p2p connectivity software on NUCLEO L152RE + X-NUCLEO-IDS01A4. We need to use auto acknowledgement and auto retransmission feature on spirit1. Whatever the application in the SUBG1 package, is not using these features. When we try to enable these features, it is not functioning properly. It would be of great help if anybody could share some test code one might have used to test these features. Symptoms: Sender is getting ack for the first packet, but not for subsequent packets. Receiver is giving tx fifo failure interrupt. Contacted ST online help, but no reply. Any help is greatly appreciated. #spirit1 #spsgrf
Posted on October 04, 2016 at 16:58Hi,I use the SPSGRF module in 868MHz Narrowband. I search to send packet with this configurations : - Fc = 869.2375MHz- Fdev = 2.7 kHz- Datarate = 4.8 kBit/s- Number of channels : 0- Spacing channel : don't care ? - Modulation : GFSK_BT05So for my receiver a set : - Channel filters : 11,0 kHz > (2*Fdev + datarate) ~ 10,4KHz- SQI / PQI : Disable - RSSI Threshold : -20 dBm.In this configuration I receive nothing. In my Spectrum analyzer, I see a signal when I transmit something, but receiver doesn't see : Preamble, Sync Word ... So which parameter I miss to configure for make a reception ? Something hide ? Or it's my transmit who is no good ? I think is not channel filter the problem... Regards,Lo�c #spirit1-rx-tx-receive-transmit
Posted on September 29, 2016 at 13:06Dear Support Team,I want to collect data from 64 heat meters, heat meters are from Danfoss, in mode T1.The purpose of the project is only data collecting from heat meters without decryption, collected data forwarding to web server. I have few questions about the ST's wireless M-bus stack?1. What is the maximum supported meter number at the same time, how many meters can I add to the collector device? Best regards Levente.
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.