Skip to main content
pouya
Associate II
Dec 8, 2016 8:13 AM UTC
Question

Removing the spwf01sx cgi files.

Posted on December 08, 2016 at 09:13

Hi, 

I was wondering that if it is possible to delete the HTML and CGI file system from the module.?

P.S: I can see from the documentation that it is possible to disable/enable the feature. My concern is to permanently delete the files.

#cgi
    This topic has been closed for replies.

    1 reply

    Gerardo GALLUCCI
    ST Employee
    Dec 10, 2016 2:17 PM UTC
    Posted on December 10, 2016 at 15:17

    Hi,

    cannot delete files inside STM32 flash (so, HTML and/or CGI). The ones marked as 'I' from AT+S.FSL command.

    You can delete HTML inside external flash, if using SPWF01Sx.11, by AT+S.HTTPDFSERASE. The ones marked as 'E' from AT+S.FSL command.

    Regards

    jerry