Visitor II
Nov 18, 2016 11:18 AM UTC
Question
WIND:55:''Pending Data...'' is generated after ''AT+S.SOCKR'' command
- 2 replies
- 818 views
Posted on November 18, 2016 at 12:18
I have been using the your WiFi module, The module desciption is below;
# nv_manuf = ST # nv_model = SPWF01SA1 # nv_serial = 4313D02202 # nv_wifi_macaddr = 00:80:E1:FF:BA:10 +WIND:1:Poweron (141106-0950875-SPWF01S) (f/w version) After socket write operation with''AT+S.SOCKR'' command, ''+WIND:55:Pending Data...'' is generated. UM1695 does not include any information about that issue. I upgrate the firmware from 3.3(141106) to 3.5(160129) I retest the module but got same result. I attached the test outputs screen shot. I already test two modules but the result is same.