Get ready for the STM32 Summit 2026 | Online, November 3
Find useful information on analog and audio applications: TDA7294-based designs, PDM to PCM noise, and SPICE models.
Most recent activity
Posted on December 23, 2012 at 23:17Good night,I'm using a TDA2822M to drive headphones in a breadboard prototype, but the problem is the amplifier that captures every RF interference such that of power switches and electric engines.Could this be a consequence of the high gain of the amplifier and the high input resistance, the circuit used was the same as suggest in the datasheet of the device.Thank you very much for your atention,Best regards,Daniel Almeida
Posted on January 02, 2013 at 19:50I'm using the TSC888A current sensing amplifier in BLDC (brushless DC) motor controller current limit circuit. I'm seeing a gain of about 10 from the amplifier instead of the published typical value of 20. The data sheet does not specify a min or max gain but does state an output accuracy of 6%. With a 0.05 ohm series resistor and 1.2A current I am seeing an output voltage of 650mV. According to my calculations I should be seeing 1.2V (1.2*0.05*20).Vcc and Vp are both connected to same 12V power bus.Has anyone else seen this problem? #tsc888
Posted on August 01, 2012 at 21:19Hi,I am working on an instrumentation amplifier circuit. I would like to perform a noise analysis on the circuit and would like to get a SPICE model for the TS9224 opamp. I am using LTSpice. I could also use some help in understanding the output I get from the noise analysis.ThanksScott Gauche #ts9224-noise-spice
Posted on June 11, 2012 at 15:45What is the definition of quiescent current parameters in operational amplifier project? Thanks, Luli #quiscent-current
Posted on May 29, 2012 at 15:24Do you have SPICE models for TSV6390AIDT and/or TSV6290AIDT? Thanks, Luli #op-amps-spice-macromodel
Posted on June 06, 2012 at 17:17I am adopting the TS922 family and I have a 16Volt rail on my PCB board. I am thinking to use a rail splitter (+/- 8Volts) or I can always step down the supply voltage if needed. The supply voltage of TS922 listed in the datasheet appears at 2.7Volts to 12Volts. Is this ±12Volts or 12Volts total?
Posted on May 30, 2012 at 18:13Does STMicroelectronics offers ADS (Advanced Design System) model developed by Agilent? #ads
Posted on May 04, 2012 at 17:05Hello,In datasheet, sometimes maximum output current is indicated (IsourceMin, Typ, Max), sometimes it is missing.What is the best method to determine if an OpAmp can supply enough current to our load?Thanks for the support,Jean #maximum-isink-isource #maximum-output-current #isource
Posted on April 06, 2012 at 10:05Dear forum members,Perhaps, you wonder what is the difference between single and dual supplies ?Or maybe if the op-amp will have the same behavior with Vcc= 0 -> 5V or Vcc= +/- 2.5V.It is important to keep in mind that all voltages have a reference. It means that we have to think : difference of potential.Most of the time, when we say Vcc=5V, it means a potential difference of 5V referenced to the GND : 0V.As a conclusion, we can deduce that both of the following configuration will have the same behavior : But, there is a point that you should take into consideration.In your application, it is not as simple as it looks like to switch from one configuration to the other one. Actually, you have to take into account all your voltages.Here you can find a simple example in order to illustrate it, if you want to switch from a configuration with Vcc= 0 -> 5V to a configuration with Vcc = +/- 2.5V : Actually, in the 2nd configuration the output vol
Posted on February 15, 2012 at 12:04Dear forum-users,If you like using ST Op-Amps, here is a simple table that will direct you quickly to the most appropriate ST Op-Amps, based on popular standard devices. ST Op Amps Standard devices Description TSV621A AD8613 Micropower Op amp LMV824 LMV824 Std Op amp TS912 / TSX712 LMC6482 16V CMOS Op amp TSV852 or TSV6392 LMV932 Gen Purpose Op amp TSV521 /TSV522 AD8541 / MCP6041 /OPA2348 1Mhz Low Power Op amp LMV321L LMV321 Gen Purpose LMV331 LMV331 Low power Comparator TSX711 LMC6481 / TLC271 /TLV271 16V CMOS Op amp TSX631 TLV2211 / LPC661 16V CMOS low power Op amp TS3011 LMV7219 / MAX999 High speed Comparator TS881 MAX9119 / LPV7215 Nano power Comparator TSZ121 OPA333 / OPA330 / LTC2054
Posted on December 05, 2011 at 11:19Hello,I would like to use macromodels to simulate my schematics but I am not able to find them.I think that they are available because in the TSV6239 datasheet it is mentioned :Two accurate macromodels (with or without shutdown feature) of the TSV629x are available on STMicroelectronics� web site at www.st.com.Thank you for your support. #macromodels #op-amps-spice-macromodel #op-amps
Posted on November 18, 2011 at 15:17 Dear Forum Members, I�d like to share a few tips on the usual process I use to select an Op Amp based on pre-defined technical requirement. The tool I use more often is the product selector, which can be accessed by clicking on the following icon from ST home page: Then select in the product tree: �Amplifiers and Comparators� > �Amplifiers�. Here is also direct link to thehttp://www.st.com/stonline/stappl/productcatalog/app?page=productSelector:http://www.st.com/stonline/stappl/productcatalog/app?page=productSelector The next step is then to use the �Filter Panel� in order to refine the technical requirements. Tip1: use the arrows to see all the filtering parameters. Tip2: use the icon close to the parameter name to toggle the filter type between �tick case� and �slider�. In my typical Op Amp selection, I would firstly apply filter on the more obvious (and restrictive) parameters, like voltage rating �Vcc�, �number of channel� or �automotive gr
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.