Skip to main content
Frederic TUPIN
Visitor II
February 15, 2012
Question

Crossref to ST Op Amps

Posted on February 15, 2012 at 12:04

Dear forum-users,

If you like using ST Op-Amps, here is a simple table that will direct you quickly to the most appropriate ST Op-Amps, based on popular standard devices.

 

ST Op Amps

 Standard devices 

Description  

 TSV621A AD8613   Micropower Op amp

 LMV824 LMV824   Std Op amp

 TS912 / TSX712 LMC6482   16V CMOS Op amp

 TSV852 or TSV6392 LMV932 

 Gen Purpose Op amp

 TSV521 /TSV522  AD8541 / MCP6041 /OPA2348  1Mhz Low Power Op amp

 LMV321L  LMV321   Gen Purpose

 LMV331  LMV331  Low power Comparator

 TSX711  LMC6481 / TLC271 /TLV271  16V CMOS Op amp

 TSX631 TLV2211 / LPC661   16V CMOS low power Op amp

 TS3011  LMV7219 / MAX999  High speed Comparator

 TS881  MAX9119 / LPV7215  Nano power Comparator

 TSZ121  OPA333 / OPA330 / LTC2054  Zero drift  Op Amp

 TSV711  OPA336  Low offset  / Vio op amp

 TSV712  OPA2336  Low offset  / Vio op amp

 TSU101  LPV521 MAX4470 MCP6441 Nano Power Op amp

 TSV521  OPA348  Energy efficient Op amp

here are listed only few of widely used devices except LM3 & LM29 series, but

please feel free to complete this table whenever you find a good Xref using ST Op-Amps.

#xref-amp-lmc6482-opa348-opa333
This topic has been closed for replies.