Skip to main content
jean_prieur
Associate III
May 4, 2012
Question

Maximum output current of an OpAmp

Posted on May 04, 2012 at 17:05

Hello,

In datasheet, sometimes maximum output current is indicated (IsourceMin, Typ, Max), sometimes it is missing.

What is the best method to determine if an OpAmp can supply enough current to our load?

Thanks for the support,

Jean

#maximum-isink-isource #maximum-output-current #isource
This topic has been closed for replies.

1 reply

Nickname14663_O
Associate
May 7, 2012
Posted on May 07, 2012 at 15:08

Dear Jean,

In most of datasheets, it is possible to find this information in the figures.

For example, here below there is the figure 6 of the TSV851 datasheet. 

It shows the output current vs the output voltage.

0690X00000602fyQAA.jpg

Thanks to this figure, you will be able to find the maximum current that the op-amp can sink or source.

Best regards,

Sylvain