cancel
Showing results for 
Search instead for 
Did you mean: 

Virtual COM port driver 1.4.0 doesn't work with CDC examples

peterdonchev
Senior
Posted on February 02, 2015 at 21:22

Hi, I have a problem with virtual com port driver 1.4.0. CDC devices are not recognized, when this driver is installed, but I don't have problem with the old driver (1.3.1) under Windows 7. I must be sure that CDC device will work under Windows 8.1. Where is the problem?

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
tsuneo
Senior
Posted on February 03, 2015 at 09:21

A) Clean up of old driver on Windows

1) Uninstall old ST's driver, if any

Control Panel - Programs and Features

- right click on ''Virtual COM Port Driver'' (STMicroelectronics)

- In the InstallSheild dialog, click on ''Remove'' check box > ''Next'' button

2) Uninstall old device instances on the Device Manager

Make a new text file, ''DevManager.bat'', and copy these two lines to the file.

set devmgr_show_nonpresent_devices=1

start devmgmt.msc

Right click above .bat file, ''run as administrator'', and the Device Manager comes up.

- enable ''Show hidden devices'' on View menu

Find this device instance(s), (your PC may have two or more)

Ports (COM and LPT)

- STMicroelectronics Virtual COM Port (COMxx)

Right click on the all of instances - Uninstall

3) Clean up DriverStrore and oemxx.inf in Windows\inf folder

Run command prompt under administrator privilege, copy these two lines (right click - paste) to the dialog.

cd %WINDIR%\inf

findstr ''VID_0483&PID_5740'' *.inf

Above ''findstr'' lists up oemXX.inf (XX: number) files, which include ST's CDC VID/PID

Delete these ''.inf'' files using pnputil (which deletes DriverStore and .pnf files, too)

pnputil -d oemXX.inf

B) Driver from Windows Update

If your PC would connect to Internet, the latest CDC driver should be automatically downloaded from Windows Update, just when a ST CDC device (VID_0483&PID_5740) is plugged in.

C) Apply VCP_v1.4.0 driver

Distributed VCP_v1.4.0.exe copies just installer folder.

You'll need to run DPINST utility in the folder explicitly.

C:\Program Files\STMicroelectronics\Software\Virtual comport driver\Win7\dpinst_x86.exe

or dpinst_amd64.exe

Tsuneo

peterdonchev
Senior
Posted on February 03, 2015 at 12:24

Thanks for the reply.

I did not have any driver installed prior 1.4.0. Nor windows update found any driver.

Only solution for me was 1.3.1. which came with the examples. Anyway, I will try to cleanup

and install again 1.4.0. I will keep you informed.

tsuneo
Senior
Posted on February 03, 2015 at 15:15

> Nor windows update found any driver.

a) VID/PID = 0x0483 / 0x5740

What is the VID/PID, assigned to the device?

Windows update (and genuine VCP_v1.4.0) matches just to the device of this VID/PID

b) Single CDC device (not composite one)

If the CDC interfaces would be part of a composite device, Windows update and VCP_v1.4.0 don't match, even on the above VID/PID

Tsuneo

peterdonchev
Senior
Posted on February 03, 2015 at 15:44

VID and PID are the same, but widows first found a composite device (two Virtual COM ports). Which is strange, because after installing 1.3.1. it become a single device. I'm compiling CDC example from

http://www.element14.com/community/servlet/JiveServlet/downloadBody/51670-102-3-272404/STM32F4DIS-BB%20Software%20Examples%2020130307.zip

.

peterdonchev
Senior
Posted on February 03, 2015 at 21:54

I tried with another computer, the result is the same.

This is what I got, after discovery board was connected (Windows Update did not found a driver).0690X00000605EWQAY.png

And after installing 1.3.1.:

0690X00000605EbQAI.png
tsuneo
Senior
Posted on February 05, 2015 at 05:32

Ah, I remember.

To get ST's CDC driver from Windows Update, The Device triad (class, subclass and protocol) of the CDC device should be (0x02, 0x00, 0x00). Windows treat a CDC device of Device triad (0, 0, 0) as you have seen. The VCP example in STM32_USB-FS-Device_Lib_V4.0.0 has correctly set it up, as follows. And then, this example finely works with Windows Update and VCP_v1.4.0

\STM32_USB-FS-Device_Lib_V4.0.0\Projects\Virtual_COM_Port\src\usb_desc.c
/* USB Standard Device Descriptor */
const uint8_t Virtual_Com_Port_DeviceDescriptor[] =
{
0x12, /* bLength */
USB_DEVICE_DESCRIPTOR_TYPE, /* bDescriptorType */
0x00,
0x02, /* bcdUSB = 2.00 */
0x02, /* bDeviceClass: CDC */ <------ OK
0x00, /* bDeviceSubClass */
0x00, /* bDeviceProtocol */

But all of other examples of ST's libraries, including the latest Cube ones, don't work with Windows Update and VCP_v1.4.0, because these examples set the Device triad to (0, 0, 0). The VCP example of STM32_USB-Host-Device_Lib_V2.1.0 should be revised, as follows,

\STM32_USB-Host-Device_Lib_V2.1.0\Project\USB_Device_Examples\VCP\src\usbd_desc.c
/* USB Standard Device Descriptor */
__ALIGN_BEGIN uint8_t USBD_DeviceDesc[USB_SIZ_DEVICE_DESC] __ALIGN_END =
{
0x12, /*bLength */
USB_DEVICE_DESCRIPTOR_TYPE, /*bDescriptorType*/
0x00, /*bcdUSB */
0x02,
0x00, /*bDeviceClass*/ <------ 0x02
0x00, /*bDeviceSubClass*/
0x00, /*bDeviceProtocol*/

Also, all of CDC_Standalone examples in STM32Cube should be revised.

\STM32Cube_FW_F0_V1.2.0\Projects\STM32072B_EVAL\Applications\USB_Device\CDC_Standalone\Src\usbd_desc.c
\STM32Cube_FW_F1_V1.0.0\Projects\STM3210E_EVAL\Applications\USB_Device\CDC_Standalone\Src\usbd_desc.c
\STM32Cube_FW_F1_V1.0.0\Projects\STM3210C_EVAL\Applications\USB_Device\CDC_Standalone\Src\usbd_desc.c
\STM32Cube_FW_F2_V1.1.0\Projects\STM322xG_EVAL\Applications\USB_Device\CDC_Standalone\Src\usbd_desc.c
\STM32Cube_FW_F3_V1.1.0\Projects\STM32373C_EVAL\Applications\USB_Device\CDC_Standalone\Src\usbd_desc.c
\STM32Cube_FW_F3_V1.1.0\Projects\STM32303C_EVAL\Applications\USB_Device\CDC_Standalone\Src\usbd_desc.c
\STM32Cube_FW_F4_V1.4.0\Projects\STM324xG_EVAL\Applications\USB_Device\CDC_Standalone\Src\usbd_desc.c
\STM32Cube_FW_F4_V1.4.0\Projects\STM324x9I_EVAL\Applications\USB_Device\CDC_Standalone\Src\usbd_desc.c
\STM32Cube_FW_L1_V1.0.0\Projects\STM32L152D_EVAL\Applications\USB_Device\CDC_Standalone\Src\usbd_desc.c
/* USB Standard Device Descriptor */
const uint8_t hUSBDDeviceDesc[USB_LEN_DEV_DESC]= {
0x12, /* bLength */
USB_DESC_TYPE_DEVICE, /* bDescriptorType */
0x00, /* bcdUSB */
0x02,
0x00, /* bDeviceClass */ <------ 0x02
0x00, /* bDeviceSubClass */
0x00, /* bDeviceProtocol */

Tsuneo
rc
Associate II
Posted on May 20, 2015 at 18:33

I did the change for device class in usbd_desc.c but in Windows (XP) I get this:

 0690X00000605H1QAI.png

I ran the 1.4 installer but perhaps it does not support XP since the driver that shows up is:

0690X00000605H6QAI.png

Is there any way to get this to work on XP?

What about on a Mac?

tsuneo
Senior
Posted on January 31, 2016 at 05:03

Clean up all of the VCP instances in trouble on your PC using USBDeview utility,

http://www.nirsoft.net/utils/usb_devices_view.html

- Run this utility

- Scroll the list to left, show up ''Vendor ID'' column

- Click on ''Vendor ID'' label --> the list is sorted by VID/PID

- Find VID/PID = 0483/5740 (in hexadecimal, 1155/22336 in decimal, shown on the source code)

- (shift-)click on the all lines of this VID/PID to select them

- right click on selected lines and choose ''Uninstall the selected devices''

On Device Manager, the VCP instances in trouble are scattered around under a couple of branches. It may be hard to find them all on Device Manager. If any one would be left, the trouble could stay in unfixed.

Try USBDeview to clean them up.

Tsuneo

Muhammad Moiz khan
Associate II
Posted on October 10, 2016 at 13:46

Hello, 

I am using STM32F070CB micrcontroller and working on USB peripheral, I want to send my data to PC through USB and want to verify the data on terminal , hence implementing VCP, I have downloaded STM32F0x2_USB-FS-Device_Lib V1.0.0 however after syncing these libraries in CooCox IDE my device is not acting as VCP.

I'm currently rectifying the issue any help in this regard would be highly appreciated.

Regards.