2018-05-21 12:08 PM
I have updated some firmware and need to flash the MC on a custom board with a STM8AL3188 and SWIM connector. This is my first project using IAR. I have browsed some tutorials and made sure the Debugger Driver was set to ST-Link. However I do not know what else is needed to establish a connection so I can download the new firmware. So I figured I'd ask the experts.
The firmware on the ST-Link was updated to 'V2.J29.S7 STM32+STM8 Debugger: via the STM32 ST-LINK utility. And I am using IAR Workbench STM8 IDE V3.10.4
For images of connector, board, and workspace. (
)Any help would be appreciated. Thanks!
#flash #st-link #stm82018-05-22 4:06 AM
'
However I do not know what else is needed to establish a connection'
At s minimum have the wires connected. And preferably have your board powered separately.
2018-05-22 10:05 AM
Yes I have done both of those steps.
2018-05-22 8:50 PM
Then you are good to go.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.