cancel
Showing results for 
Search instead for 
Did you mean: 

What is the CubeMX2 WWDG 'Time Unit' meaning?

Hello,

 

I am developing an app that uses the Window Watchdog (WWDG). In the CubeMX2 (version 1.0.1) WWDG configuration, there is a field called 'Time Unit'. I set this field to 'Milliseconds', then set a 'Min Time' of 80 and a 'Max Time' of 233, enable the early interrupt, and generate the code. I then compile my app, and it works as expected. If I return the CubeMX2 and set the 'Time Unit' field to 'Seconds', keep the 'Min Time' and 'Max Time' the same as before, and I regenerate the code, I don't get any code changes, just changes in the ioc2 file. See ioc2 diff in the attachment.

 

May I get an explanation of what the 'Time Unit' means?

Thank you,

-Gil

0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.