Skip to main content
Associate II
September 19, 2024
Solved

FLASH.ld syntax error when upgrading to CubeMX v6.12.1

Hello,

Since the latest release of CubeMX (6.12.1), I have been encountering syntax errors related to the "FLASH.ld" file. This issue only arises when I generate code while setting the Toolchain/IDE to CMake. I am using STM32H753IIKx. It seems that CubeMX does not specify which RAM to use when setting the Toolchain/IDE to CMake.

I have also included the FLASH.ld file that was generated for your reference.

 

Thanks for your help.

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
December 2, 2024

Hello @OmidES 

Issue has been solved on the STM32CubeMX V6.13.0.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

45 replies

STTwo-32
ST Technical Moderator
September 20, 2024

Bonjour @OmidES 

Could you please attach you .ioc file (if possible for the two CubeMX versions).

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
OmidESAuthor
Associate II
September 20, 2024

Bonjour,

Yes, sure. I have attached the two versions.

Another issue that I also faced, in CubeMX 12.6.0, was when I set the Toolchain to CMake, the DTCMRAM is used. However, if I change the Toolchain to STM32CubeIDE, the RAM_D1 is being used. Is there a way to select which RAM to use in CubeMX?

Thanks again for your help.

Visitor II
September 21, 2024

it seem like a bug。 the same configuration,  6.12.0 works well. but  6.12.1 have ld error

LLeva.1
Associate II
September 28, 2024

Confirmed with regular "make".

Missing "RAM" in .ld file. When I repair the file, next cubeMX code generation breaks it again:

 

 

ENTRY(Reset_Handler)

/* Highest address of the user mode stack */
- _estack = ORIGIN(RAM) + LENGTH(RAM); /* end of RAM */
+ _estack = ORIGIN() + LENGTH(); /* end of RAM */
/* Generate a link error if heap and stack don't fit into RAM */
_Min_Heap_Size = 0x200; /* required amount of heap */
_Min_Stack_Size = 0x400; /* required amount of stack */


@@ -143,7 +143,7 @@ SECTIONS

 . = ALIGN(4);
 _edata = .; /* define a global symbol at data end */
- } >RAM AT> FLASH
+ } > AT> FLASH

 
 /* Uninitialized data section */

@@ -160,7 +160,7 @@ SECTIONS
 . = ALIGN(4);
 _ebss = .; /* define a global symbol at bss end */
 __bss_end__ = _ebss;
- } >RAM
+ } >

 /* User_heap_stack section, used to check that there is enough RAM left */
 ._user_heap_stack :

@@ -171,7 +171,7 @@ SECTIONS
 . = . + _Min_Heap_Size;
 . = . + _Min_Stack_Size;
 . = ALIGN(8);
- } >RAM
+ } >

 

c:/program files (x86)/gnu arm embedded toolchain/arm/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld.exe:STM32F446RCTx_FLASH.ld:56: syntax error
collect2.exe: error: ld returned 1 exit status

Adding "RAM" back to ld will fix it.

 

Thanks GITHUB for keeping proper version! Interesting, old bugs are still here? When we'll get hotfix? And I don't want to hear about "concerned team for investigation".

     
OmidESAuthor
Associate II
September 28, 2024

I found a quick solution. You can generate the code by setting the Toolchain to STM32CubeIDE. Then make a copy of the .ld file and use it on your project. Becausae the .ld file generated when setting Toolchain to STM32CubeIDE is still correct.

I hope that helps.

Visitor II
September 30, 2024

In STM32CubeMX, just click on "TOOLS"  menu then select both:

eduard0claudi0_0-1727655747986.png

Save project and re-generate it. The linker file will be correct



Visitor II
September 30, 2024

I WAS WRONG! Sorry ....

The correct action is to select FLASH (or RAM) in "Search an Application Region" :

eduard0claudi0_0-1727657469535.png

Then save and re-generate project.

:(

Visitor II
September 30, 2024

Well, this is not the solution either. In my case, for STM32F103C8Tx, CubeMX does not allow configuring it's memories (under tools).

CubeMX produces an .ld file completely different when exporting for Makefiles and exporting with build files for STM32CubeIDE. Strangely, the .ld file produced for using with STM32CubeIDE reports it is generated by STM32CubeIDE and not by MX.


Code_EPYhY8Je3o.png



FYI, I am attaching the two different linker files

Associate
October 4, 2024

Wow, this is so frustrating. I lost the better part of a day's work due to this bug. Not so much lost code, but lost time, trying to figure out what I'd done wrong in my project. To then finally discover it's not anything I did wrong, but rather it's a bug in CubeMX. Lame. 

For anyone experiencing this issue, here's what I did to resume productivity. 

  1. Removed CubeMX 6.12.1
  2. Restored from git to get my project prior to the point where 6.12.1 migrated my ioc file
  3. Installed CubeMX 6.12.0
  4. Somewhat painfully got my project back to where it was before 6.12.1 (despite frequent git commits)

The take away is: do frequent git commits, and never trust that letting CubeMX migrate your project isn't going to break something. The irony for me was, I'd updated CubeMX due to a bug in the version I'd been running (fields in the app would suddenly become non-responsive to keyboard input). 

 

 

 

 

Visitor II
October 5, 2024

Another option (but not without risk), you can edit the IOC file and change the mininum cubemx required version, I am pretty sure they did not change anything between 6.12.0 and 6.12.1 they just broke the tool

grzegorz
Associate III
October 7, 2024

CubeMX forgets about references to RAM

We have:

_estack = ORIGIN() + LENGTH();    /* end of RAM */

Should be

_estack = ORIGIN(RAM) + LENGTH(RAM);    /* end of RAM */

And at the end of .data section definition:

  } > AT> FLASH

Should be:

  } >RAM AT> FLASH

Also for .bss

  } >

Should be:

  } >RAM

And for ._user_heap_stack we have:

  } >

Should be:

  } >RAM
karolalexandersecret
Associate II
October 24, 2024

Thanks a lot Grzegorz,

 

Your answer helped me on two separate project ! Hope the next version of cubeMX come soon

Visitor II
October 19, 2024

When the fixed version will be released

Andrew Neil
Super User
October 19, 2024
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
RichardS1
Associate II
November 25, 2024

Certified ST software quality moment.

Imagine how trivial it is to test this thing before pushing it to thousands of users.

Please, increase you QA budget at least.

This is a nightmare...

Graduate
November 26, 2024

Exactly, they would have just needed an auto-build process in their build pipeline, but it seems they don't have any, otherwise this bug wouldn't have made it to the release...