2025-05-25 4:09 AM
I am about to integrate Ezurio sna module If 513 with the STM32MP257F-EV another to provide wireless capabilities to my board. does any one try this before for any assistance. I am using mini PCIE TO M.2 adapter to connect. so if there is any to assist me with a complete guide , I will appreciate,
Thank you.
2025-05-25 5:49 AM
Have you already set up Linux on the board? If you plug the module into the miniPCIe and run lspci, will it show up?
2025-05-25 6:18 AM
the only thing I see is 00:00.0 PCI bridge: Synopsys, Inc. Device 0550 (rev 01)
2025-05-25 12:18 PM
And you see the same without the module connected (and powered up)?
Can you connect the module to some other host system and compare results?