Skip to main content
ST AME Support NF
ST Employee
Nov 16, 2021 10:08 AM UTC

How to redirect the printf function to a UART for debug messages

Introduction

It can be especially useful during code development to display messages in a terminal window about various system parameters to help with debugging. An easy way to do that is to use the printf function and redirect the output to a UART for display in a terminal window.

The STLINK embedded on ST Nucleo boards have a virtual COM port feature, and we can easily get debugging information on a terminal using printf redirected to the UART of the STM32 connected to the STLINK pins used for the virtual COM port.
In this article, I show you how to redirect the printf output to the STM32 UART peripheral that connects to the UART pins on the embedded STLINK. It transmits to the host computer and displays via a Windows terminal program, Tera Term.
 

1. Prerequisites

Hardware

  • Micro USB cable: in order to power and program the board
  • NUCLEO-G070RB

1891.png
 
Software

2. Theory

On the NUCLEO-G070RB board, the embedded ST-LINK/V2 is connected to PA2 (UART TX) and PA3 (UART RX) of the target STM32G070 device. 

These port pins have USART2 alternate functions. Printf is redirected to use PA2 and PA3. We then use a terminal connected to the virtual COM port of the ST-LINK of the Nucleo board to display the printf messages.
 

3. Steps

  1. Open STM32CubeIDE
  2. Create a new project using the NUCLEO-G070RB board


3. steps 1.png
 

  1. Give a name to the project
  • For this example, the project name is “Printf”.

3. steps 2.png
 

  1. Initialize all peripherals with their default settings:
  • To do this, click on [Yes].

3. steps 3.png
 

  1. Make sure that USART2 has been selected, configured, and mapped to PA2 and PA3 as shown below:
  • By default, this was configured when starting the project from the Nucleo board that was selected.
  • First make sure that USART2 is activated as shown here:


3. steps 4.png

 

  • It should be configured in Asynchronous mode with the following settings as shown below in the red rectangles:

 

3. steps 5.png

 

  • Make sure the USART2 alternate functions have been mapped to PA2 and P3 that are connected to the TX and RX pins (respectively) of the ST-LINK on the Nucleo board.

 

3. steps 6.png

  1. Generate the code
  • Saving the project generates the code.
  1. Add code for printf:
  • This code redirects the output of the printf function to the USART2. The printf function is calling fputc to transmit the output via the USART.
  • In main.c, add the following code:
/* USER CODE BEGIN PFP */
#define PUTCHAR_PROTOTYPE int __io_putchar(int ch)
/* USER CODE END PFP */
…
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 printf("Hello World\n\r");
 HAL_Delay(1000);
 /* USER CODE END WHILE */

…
/* USER CODE BEGIN 4 */
/**
 * @brief Retargets the C library printf function to the USART.
 * None
 * @retval None
 */
PUTCHAR_PROTOTYPE
{
 /* Place your implementation of fputc here */
 /* e.g. write a character to the USART1 and Loop until the end of transmission */
 HAL_UART_Transmit(&huart2, (uint8_t *)&ch, 1, 0xFFFF);

 return ch;
}

/* USER CODE END 4 */
  1. Build the project, enter debug mode, and run the code.

3. steps 7.png

To execute the code:

  • Enter the debug session.

3. steps 8.png

 

  • Execute the code.

 

3. steps 9.png

 

  • Open a terminal application like Tera Term.
  • Configure the serial port connection to the STLINK virtual COM port.

 

3. steps 10.png

 

  • Select the following settings.

 

1902.png

 

  • You now see the printf message, “Hello World”, being displayed every second.

 

1903.png

 

4. Related links

5. Notes

5.1 Tips when using C++

We need to update the _write and _read functions,

namespace std{
#ifdef __cplusplus
extern "C"{
#endif
int _write(int fd, char *ptr, int len){
 (void)fd;
 int i;
 for(i=0;i<len;i++){
 uart_write(*ptr++);
 }
 return len;
}

size_t _read(int fd, char *ptr, size_t len){
 (void)fd;
 size_t i;
 for(i=0;i<len;i++){
 *ptr++ = uart_read();
 uart_write(*ptr++); //For Terminal Echo
 }
 return i;
}

#ifdef __cpluscplus
}
#endif
}

And the main function.

int main(){
 setbuf(stdin,NULL); //TO HANDLE INPUT BUFFER WHEN USING SCANF/COUT
 printf("\rHello World\n\r");
 while(1);
}

5.2. Line-buffering

The default (well, GCC's default) is that stdout is line-buffered, that is, the output is not sent until a complete line has been formed.

This affects that the output does not actually appear until a new line is sent, for example:

printf( "Hello, " ); // No output here ...
printf( "World!" ); // ... still no output ...
printf( "\n" ); // Now the output appears!

This is a common cause of confusion, as many people expect that the output should appear immediately.

It is also worth noting that, by default, stderr is not line-buffered - so output does appear "immediately," for example:

fprintf( stderr, "Hello, " ); // output *does* appear here ...
fprintf( stderr, "World!" ); // ... and here ...
fprintf( stderr, "\n" ); // and here!
 

26 replies

nicolas
Senior II
May 21, 2024 3:08 PM UTC

A terminal application is not necessary, it can be done inside STM32CubeIDE:

https://community.st.com/t5/stm32-mcus/how-to-use-the-stm32cubeide-terminal-to-send-and-receive-data/ta-p/49434

XR.1
Senior
Sep 24, 2024 9:00 PM UTC

Awesome!

Andrew Neil
Super User
Oct 21, 2024 2:28 PM UTC

Before trying to get printf working, be sure that the basic UART transmission is working - see:

https://community.st.com/t5/stm32-mcus/implementing-uart-receive-and-transmit-functions-on-an-stm32/ta-p/694926 

 

PS:

For an example of what can go wrong, see here!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
carlosdelfino
Senior
Jan 18, 2025 3:08 AM UTC

it worked perfectly on the Nucle-f411re.

Now the STM32 world opens up to great challenges.

Buy me a coffeeMy Portal about Analog ElectronicsMy Youtube Channel where I share my learning about Analog Electronic
Explorer II
Oct 31, 2025 5:23 AM UTC

Still newbie here!

I'm trying to implement this in C++ and am not sure what to do with the section "5.1 Tips When Using C++." Do I just add those lines at the end of "syscalls.c" to update the _write and _read functions? Or do I need to replace it?

XR.1
Senior
Nov 5, 2025 2:14 AM UTC

Hi!

Try this alternative, also from ST (it worked for me):

https://community.st.com/t5/stm32-mcus/how-to-redirect-the-printf-function-to-a-uart-for-debug-messages/ta-p/49865

 

First of all, make it work for C, then you can freely move it onto C++. In the same tutorial there are instructions for C++.