cancel
Showing results for 
Search instead for 
Did you mean: 

X-NUCLEO-WB05KN CN7 cts/rts don't work

dd1337
Associate

Hi I'm trying to connect NUCLEO-H755ZI-Q with X-NUCLEO-WB05KN via usart. I'm using usart2 (pd3, pd4, pd5, pd6) on the host board and CN7 on the shield. BLE initialisation fails if I set `hw-flow-control` in Zephyr in devicetree. Without flow control and with the same connection, it works fine. I'm using BLE_TransparentMode_UART_with_Updater from X-CUBE-wb05n. I tried soldering SB10 and SB11, but to no avail. It would be great to have a full datasheet with a detailed description of all interfaces and how they work, the only document I could find is UM3355, which is not very helpful.

 

1 REPLY 1
STTwo-32
ST Employee

Hello @dd1337 

The datasheet is available only for the MCUs. Since the X-NUCLEO-WB05KN1 is based on the STM32WB05KN that have the DS14620 as datasheet. For the Zephyr communication. You may have a look at this issue on Github.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.