cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB Does master hold slaves MAC address?

DS.4
Senior II

Slave can configure his MAC address either in the payload or internally. This I know.

My question is , after connection, does the masters packets hold that (slaves) MAC address?

Can Slave extract (its own) MAC address from the Masters packets?

If, so , how can slave get hold of this data from code?

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
DS.4
Senior II

Thanks, does CPU2 has an event for CPU1 in case of a CONNECT_REQ packet?

I am using the BleHeartRateFreeRTOS example.

If not, how can I get hold of that packet?

Remi QUINTIN
ST Employee

Yes! this is the HCI_LE_CONNECTION_COMPLETE_EVENT event that is processed via the hci_le_connection_complete_event (...) function.

The LE Connection Complete event indicates to both of the Hosts forming the

* connection that a new connection has been created. Upon the creation of the

* connection a Connection_Handle shall be assigned by the Controller, and

* passed to the Host in this event. If the connection establishment fails this

* event shall be provided to the Host that had issued the LE_Create_Connection

* command.

* This event indicates to the Host which issued a LE_Create_Connection command

* and received a Command Status event if the connection establishment failed

* or was successful.

DS.4
Senior II

Hi, almost there,

On HCI_LE_CONNECTION_COMPLETE_EVENT I get this payload:

Payload 20002d7c: 

01 FF FF FF F4 02 03 20 F4 02 03 20 90 2D 00 20 3F F0 00 08 A5 A5 A5 A5 00 00 00 00 A5 A5 A5 A5 49 DC 00 08 A5 A5 A5 A5 A5 A5 A5 A5 00 00 00 00 68 00 00 80 E4 2C 00 20 00 00 00 00 94 1B 00 20 94 1B 00 20 B0 2D 00 20 8C 1B 00 20 20 00 00 00 00 00 00 00 00 00 00 00 B0 2D 00 20 00 00 00 00 18 00 00 00

Then the PDU is at 0x200302F4:

74 01 00 20 74 01 00 20 04 3E 13 01 00 01 08 01 00 2A 6A CF 50 A0 00 07 00 00 00 0A 00 07 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

2A 6A CF 50 A0 00 is the the clients address.

According to picture it should be the 6 previous bytes, but that is not my (=server) address.

Where can I see my address?