cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to debug both AppliSecure and AppliNonSecure on the STM32N6570-DK

Nakt20
Associate

I created a sample project using the STM32N657-DK,

but when I try to debug using ST-LINK, each project does not work and results in a HardFault or similar error.

I also tried loading them simultaneously from the debug configuration, but it was not successful.

How can I properly debug both AppliSecure and AppliNonSecure?

 

Also, is this the correct way to create a sample using the TrustZone feature of the STM32N6570-DK?

I would appreciate your guidance.

I am using STM32CubeIDE version 1.19.0.
For the sample project I created, I made "FSBL", "AppliNonSecure", and "AppliSecure".

 

0 REPLIES 0