cancel
Showing results for 
Search instead for 
Did you mean: 

Where is STM32L152RE datasheet?

sbmeirow
Associate II
Posted on February 19, 2014 at 09:44

The new Nucleo board lists a STM32L152RE on it, but I can't find a STM32L152RE datasheet for the microcontroller on st.com.  I did find datasheets for STM32L152R* parts with less memory, but I can't find STM32L152RE anywhere on st.com except for the Nucleo related webpages and documents.

http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/LN1847/PF260002

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
chen
Associate II
Posted on February 19, 2014 at 10:30

Hi

Yes, there does not appear to be a data sheet for the STM32L152RE part (yet)

The reference manual :

http://www.st.com/stonline/stappl/resourceSelector/app?page=fullResourceSelector&doctype=reference_manual&SeriesID=1374

and programmers manuals :

http://www.st.com/stonline/stappl/resourceSelector/app?page=fullResourceSelector&doctype=programming_manual&SeriesID=1374

Any help?

Hakim JAAFAR
Associate II
Posted on February 19, 2014 at 15:15

Hi Steve,

The datasheet you are looking for will be available on 5th March(latest revision). In the mean time you can use the one of the STM32L152RDT6 (384KB FLash / 48KB RAM) device.

Both of them are dual bank flash. Power mode are the same (active, sleep, LP-Run .... stop, standby).

Hakim.

http://www.st.com/web/en/resource/technical/document/datasheet/DM00034689.pdf

sbmeirow
Associate II
Posted on February 19, 2014 at 22:03

Thanks

Miguel CASTRO
ST Employee
Posted on February 24, 2014 at 10:48

Hi Steve,

Here is related web page on ST web:

http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1295/LN962/PF259539