2015-11-22 8:33 AM
hi there!
writing fine to SPI slave, however, when trying to read, writing stops working: for(;;){ for (i=0; i<=128; i++){ Pot0Write(i); Pot1Write(i); // res0=Pot0Read(); // res1=Pot1Read(); printf(''%5d: POT0 %d\t POT1 %d\n\r'',i,res0,res1); osDelay(10); }void Pot0Write(int data){ HAL_GPIO_WritePin(GPIOD, GPIO_PIN_1, GPIO_PIN_RESET); //set CS line active low HAL_SPI_Transmit(&hspi2,(uint8_t *)&pot0Write,1, 0); HAL_SPI_Transmit(&hspi2,(uint8_t *)&data,1, 0);// HAL_SPI_TransmitReceive(&hspi2,(uint8_t *)&pot0Write , &RxData, 1,0);// HAL_SPI_TransmitReceive(&hspi2,(uint8_t *)&data , &RxData, 1,0); HAL_GPIO_WritePin(GPIOD, GPIO_PIN_1, GPIO_PIN_SET); //reset CS line active high}/** * @brief writes to MCP4231 first sends a address/command, then data * @param None * @retval None */void Pot1Write(int data){ HAL_GPIO_WritePin(GPIOD, GPIO_PIN_1, GPIO_PIN_RESET); //set CS line active low HAL_SPI_Transmit(&hspi2,(uint8_t *)&pot1Write,1, 0); HAL_SPI_Transmit(&hspi2,(uint8_t *)&data,1, 0); // HAL_SPI_TransmitReceive(&hspi2,(uint8_t *)&pot0Write , &RxData, 1,0); // HAL_SPI_TransmitReceive(&hspi2,(uint8_t *)&data , &RxData, 1,0); HAL_GPIO_WritePin(GPIOD, GPIO_PIN_1, GPIO_PIN_SET); //reset CS line active high}/** * @brief writes to MCP4231 first sends a address/command, then reads the data * @param None * @retval None */uint8_t Pot0Read(void){ uint8_t RxData; HAL_GPIO_WritePin(GPIOD, GPIO_PIN_1, GPIO_PIN_RESET); //set CS line active low HAL_SPI_Transmit(&hspi2,(uint8_t *)&pot0Read,1, 0); HAL_SPI_Receive(&hspi2,&RxData, 1, 5000); HAL_GPIO_WritePin(GPIOD, GPIO_PIN_1, GPIO_PIN_SET); //reset CS line active high return RxData;}/** * @brief writes to MCP4231 first sends a address/command, then reads the data * @param None * @retval None */uint8_t Pot1Read(void){ uint8_t RxData; HAL_GPIO_WritePin(GPIOD, GPIO_PIN_1, GPIO_PIN_RESET); //set CS line active low HAL_SPI_Transmit(&hspi2,(uint8_t *)&pot1Read,1, 0); HAL_SPI_Receive(&hspi2,&RxData, 1, 5000); HAL_GPIO_WritePin(GPIOD, GPIO_PIN_1, GPIO_PIN_SET); //reset CS line active high return RxData;}