cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F76xx/STM32F77xx reference manual speed inconsistencies?

Richard Peters
Associate II
Posted on November 21, 2016 at 10:14

The STM32F7xx microcontrollers have a maximum operating frequency of 216 MHz. However, the reference manual of the STM32F76xx/STM32F77xx (RM0410 rev 2) mentions lower speeds at several places, which might be inconsistencies which I'd like to be verified.

At pag 150, Figure 12 ''Clock tree'' in section 5.2 ''Clocks'', the SYSCLK, Cortex core, and HCLK are all advertised as 200 MHz max. I suppose this should read 216 MHz instead?

At page 1786, ''Ethernet MAC MII address register'', the clock range of setting 100 is advertised as HCLK/102 and valid for 150-168 MHz. I suppose that, given the other ranges, this setting is valid for the 150-216 MHz range? Otherwise it would not be possible to use ethernet on a controller which runs at 216 MHz. That would be consistent with the values shown in table 276 at page 1716.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Nesrine M_O
Lead II
Posted on November 22, 2016 at 10:16

Hi peters.richard,

You are right, Thank you for bringing this issue to our attention.

It is noted and will be fixed in coming release of the document.

-Syrine-