2018-07-25 10:12 PM
2018-07-25 10:14 PM
how to flush the FIFO in the SPI RX buffer.
2018-07-25 11:06 PM
I used,
//test the rx fifo level and flush any residual data
while(LL_SPI_GetRxFIFOLevel(SPI2) != LL_SPI_RX_FIFO_EMPTY)
{
LL_SPI_ReceiveData8(SPI2); //read to empty fifo
}The other "gotcha" I found was that after configuring for 8 bit transfers, you have to independently set the FRXTH bit in CR2 so that received data is flagged after a single byte is received.
//SPI2 is on APB1 54 MHz : this configures for 8 bit byte transfers
SPI_InitStructure.TransferDirection = LL_SPI_FULL_DUPLEX;
SPI_InitStructure.Mode = LL_SPI_MODE_MASTER;
SPI_InitStructure.DataWidth = LL_SPI_DATAWIDTH_8BIT;
SPI_InitStructure.ClockPolarity = LL_SPI_POLARITY_HIGH; //clock rests high
SPI_InitStructure.ClockPhase = LL_SPI_PHASE_2EDGE; //slave latch data on rising edge
SPI_InitStructure.NSS = LL_SPI_NSS_SOFT;
SPI_InitStructure.BaudRate = LL_SPI_BAUDRATEPRESCALER_DIV32 ; //54MHz / 32 ~ 1.6875 MHz
SPI_InitStructure.BitOrder = LL_SPI_MSB_FIRST;
SPI_InitStructure.CRCCalculation = LL_SPI_CRCCALCULATION_DISABLE;
SPI_InitStructure.CRCPoly = 7;
LL_SPI_Init(SPI2, &SPI_InitStructure);
//set CR2 bit FRXTH (so that RXNE is generated on reception of 8 bit)
LL_SPI_SetRxFIFOThreshold(SPI2, LL_SPI_RX_FIFO_TH_QUARTER);
2018-07-26 5:58 AM
I just do two quick 16-bit reads of the Data Register at a point I know nothing's being clocked in at the same time. The FIFO's only 32 bits deep and it does no harm to read it if it's already empty.