cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4Discovery external interrupt problem

l_
Associate
Posted on May 13, 2013 at 15:46

Hello,  I have a problem with external interrupts on STM32F4Discovery triggered via push-button. The button is connected to pin PA4 using the same technique used for USER button (the picture is from the user manual):  http://imgimageshack.us/img248/8849/stm32f4discoveryuserbut.png  The external interrupt is generated and the switch button performs its function, but the problem is that the interrupt is generated not only via pushing the button, but for example by touching only one of the legs of the push-button with a multimeter probe or by touching certain individual pins (not short circuiting several pins with a probe, but touching only one) on the board (e.g. PORTA pins, which are left unconfigured in the code). I am posting the relevant code portion:  void

EXTI4_IRQHandler(

void

){

if

(EXTI_GetITStatus(EXTI_Line4) != RESET)

{

GPIO_ToggleBits(GPIOD, GPIO_Pin_14);

EXTI_ClearITPendingBit(EXTI_Line4);

}

}

void

init_func(

void

){

//output omitted 

RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);

//pin init

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;

GPIO_Init(GPIOA, &GPIO_InitStructure);

SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOA, EXTI_PinSource4);

//exti4 init

EXTI_InitStructure.EXTI_Line = EXTI_Line4;

EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;

EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising;

EXTI_InitStructure.EXTI_LineCmd = ENABLE;

EXTI_Init(&EXTI_InitStructure);

//nvic exti4 init

NVIC_InitStructure.NVIC_IRQChannel = EXTI4_IRQn;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x0F;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x0F;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure);

//output omitted 

}

Perhaps you can help? 

#stm32f4discovery

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on May 13, 2013 at 16:04

Perhaps you can help?

Sounds more of an issue with your hardware, than the software.

Chances are you have a grounding issue, or one with the meter changing the potential on the pins (other pins impacted via the IO ring supply). Consider wiring the switch the other way, ie normally pulled high, button closed to ground, and reverse the logic on the EXTI (falling)
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..