cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429I Discovery LCD Pin disconnected/malfunctioning

H UQ
Associate II
Posted on February 21, 2014 at 13:29

I have developed LCD driver for STM32F429I Discovery board using RGB565 (16bit) Pixel Format. My demo is displaying RED color filled rectangles by setting each RED pin (Total 5) one by one. i.e. 0x8000, 0x4000, 0x2000, 0x1000 and 0x0800 respectively.

Color displayed against 0x4000 is much closer to BLACK rather than RED. It appears either Second Last pin/bit (Second MSb) is either physically not connected or malfunctioning.

I have also tried ST Sample Code demo (LTDC ColorKeying) but behavior is same. After line number 87 of main.c file (Projects\Peripheral_Examples\LTDC_ColorKeying), Put following code to see behavior of LCD.

/////////////////////////

int x;

unsigned short Ymin, Ymax, Xmin, Xmax;

for (x = 0; x < 8; x++)

{  

    Ymin = x*40;

    Ymax = Ymin + 40;

    Xmin = 0;

    Xmax = 239;

    Rectangle_Draw(Ymin, Ymax, Xmin, Xmax, (0x8000>>x)); // Function written below

}

// Function to Draw rectangle

void Rectangle_Draw(unsigned short Ymin, unsigned short Ymax, unsigned short Xmin, unsigned short Xmax, unsigned short col)

{

    unsigned short          *add = (unsigned short *) (LCD_FRAME_BUFFER);

    unsigned short          x, y;

    for(x=Xmin; x<Xmax; x++)

        for(y=Ymin; y<Ymax; y++)

            *(add + (y*240) + x) = col;

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
H UQ
Associate II
Posted on March 04, 2014 at 08:17

PB0 (Red3) and PB1 (Red6) have been configured for Alternate Function 14 in Sample Code (LTDC_ColorKeying and LTDC_Display_2Layers examples). It should be Alternate Function 9.

PG10 (Green3) and PG12 (Blue 4) have been configured for Alternate Function 14 in Sample Code (LTDC_ColorKeying and LTDC_Display_2Layers examples). It should be Alternate Function 9.

PC10 (R2) should be configured for Alternate Function 14. It is commented in Sample Code.