2012-04-02 2:50 AM
Hi ,
I like to know if I have the possibility to connect a webcam to map stm32f4 via micro USB port, or via the camera interface card thank you for helping me2012-04-09 12:45 AM
Hy, I use it with RGB cam through DCMI cell. by
2012-04-28 7:51 AM
russian text:
Здрав�?твуйте го�?пода!Я тоже пытаю�?ь подключить WEBCAM к STM32F105/107 у которых е�?ть USB HOST. �?а данный момент удало�?ь вы�?�?нить то что обмен нужно ве�?ти по протоколу UVC. Суще�?твует ли готова�? библиотека?English text:Helloladies and gentlemen
!
I too
am trying to
connect
to the
WEBCAM
STM32F105/107
that have
USB HOST.
At the moment
we found out
is
that the exchange
should be conducted
via
UVC.
Is there a
library of
ready-made
?