cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F107 as a USB Virtual COM Port Device

ron
Associate
Posted on March 14, 2014 at 21:29

If I set up the STM32F107 as a USB Virtual COM Port Device (using for instance ''stm32_f105-07_f2_f4_usb-host-device_lib.zip''), do I need to install the Virtual COM Port driver for it to function with Windows 7?

UM1021 which describes the above firmware package indicates that the VCP driver is required, but I'm wondering if that was based on perhaps WinXP, and maybe the driver is built-in to Win7?

Any comments would be most appreciated.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on March 14, 2014 at 21:49

No, I'm pretty sure you're going to have to install the appropriate 32-bit or 64-bit driver for Win7

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..