cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103 BootLoader Go command

bsy006
Associate II
Posted on January 15, 2009 at 13:39

STM32F103 BootLoader Go command

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
bsy006
Associate II
Posted on May 17, 2011 at 12:59

Hello, I'm using STM32F103, have a problem to start go RAM downloaded code.

Connect by serial. Read memory, Download, all other commands to BootLoader work OK - reply as explained in AN2606.

After 'go' command, it doesn't look it starts. I try to download easiest code (40 bytes) which should change memory, so I could then see the result,

but nothing happens.

'Go' command returns ACK 2 times, after command itself, and after address.

BootLoader v 2.0.

[ This message was edited by: YuSh on 13-01-2009 19:31 ]

bsy006
Associate II
Posted on May 17, 2011 at 12:59

Hi, Johan,

could you tell me what is the code you succeded to start from RAM, by BL 'GO' command ?

Till now, I had no code, even easiest, gives sign of starting to run.

If you have some code do start, it may help to understand the problem.

With regards,

Yuri.

johan239955_st
Associate II
Posted on May 17, 2011 at 12:59

I can just say that I've had the same problems. However, for me it works for some applications but not for others.

The applications that I can't start from the bootloader, works if I reset the device and boot from flash instead...

Is this a documented bug, or are we doing something wrong?