cancel
Showing results for 
Search instead for 
Did you mean: 

stemwin problem

askari.nima
Associate II
Posted on February 23, 2016 at 06:48

I use stm32f407zg and stemwin library and freertos.

when I want load BMP , my microcontroller gose to HardFault after put some pixel on lcd( about half or less).

FRESULT resultBMP;

unsigned char _acBuffer[4096];

FIL * phFile;

FIL imageFile;

uint32_t NumBytesRead;

int _GetDataSD(void * p, const U8 ** ppData, uint16_t NumBytesReq, U32 Off) {

  

  

  phFile = (FIL *)p;

  // Check buffer size

  if (NumBytesReq > sizeof(_acBuffer)) {

    NumBytesReq = sizeof(_acBuffer);

  }

  // Set file pointer to the required position

 resultBMP = f_lseek(phFile, Off);

  // Read data into buffer

  resultBMP = f_read(phFile, _acBuffer, NumBytesReq, (uint32_t *)&NumBytesRead);

if(NumBytesRead < NumBytesReq)

f_close(phFile);

  // Set data pointer to the beginning of the buffer

  *ppData = _acBuffer;

  // Return number of available bytes

  return NumBytesRead;

}

//////////////////////////////////////////////////////////////////////////////////////////////////

//================================================================================================

//////////////////////////////////////////////////////////////////////////////////////////////////

void MyGui_Draw(char * sFilename)

{

  resultBMP = f_open(&imageFile, sFilename , FA_READ);

if(resultBMP == FR_OK)

    GUI_BMP_DrawEx(_GetDataSD, &imageFile,100,100);

  f_close(&imageFile);

  

}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0