cancel
Showing results for 
Search instead for 
Did you mean: 

SPI communication basic STM32F103ZE

amitwadje
Associate
Posted on June 03, 2014 at 09:24

Hello,

This is my first time I am working on STM, previously I successfully work on PIC32.

I want really basic information about SPI communication in STM32F103ZE.

my questions are,

1. How to set the SPI mode, which register ? (STM datasheets are so different than PIC, i didn't find clear info)

 2. What library file? can you please specify any SPI libraries ?  

Thank you.

   
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
chen
Associate II
Posted on June 03, 2014 at 10:45

Hi

'' 2. What library file? can you please specify any SPI libraries ?''

ST provide a whole library for all the peripherals in the processor, they call it the Standard Peripheral Libray.

It can be download here :

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/PF257890

If it is like the library for the STM32F4 parts, the library file contains examples for all the peripherals (including the SPI).

In addition, all the software samples for this device are here :

http://www.st.com/stonline/stappl/productcatalog/app?page=partNumberSearchPage&levelid=LN1565&parentid=1743&resourcetype=SW

amitwadje
Associate
Posted on June 04, 2014 at 02:18

Thank you for reply..

Can you tell me how to initialize the SPI ?

Thank you 

Posted on June 04, 2014 at 03:17

STM32F10x_StdPeriph_Lib_V3.5.0\Project\STM32F10x_StdPeriph_Examples\SPI\SPI_FLASH

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..