2015-09-30 12:15 AM
To start with, I know usart problems are common and I've read lots of threads and other sources trying to find whats wrong but I don't see it. Anyone here see anything to correct?
/*Enable USART6 clock*/
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART6, ENABLE);
/*GPIO stuff*/
RCC_AHB1PeriphClockCmd(RCC_GPIOC, Enable);
GPIO_InitTypeDef GPIO_InitStructure; //setup GPIO_InitStructure
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7;
GPIO_InitStructure.GPIO_Mode = GPIO_AF_USART6;
GPIO_InitStructure.GPIO_Speed = GPIO_Fast_Speed;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(USART6,
&GPIO_InitStructure);
/*Connect pins to alternate function, ie USART*/
GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_USART6);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_USART6);
/*Initialization of USART */
USART_InitTypeDef USART_InitStructure; //setup UART_InitStructure
USART_ClockInitTypeDef USART_ClockInitStructure; //setup UART_ClockInitStructure
USART_ClockStructInit(&USART_ClockInitStructure);
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_Init(USART6, &USART_InitStructure);
USART_ClockInit(USART6, &USART_ClockInitStructure);
USART_Cmd(USART6, ENABLE);
After this initialization we write with:
while (USART_GetFlagStatus(USARTx, USART_FLAG_TXE) == RESET);
USARTx->DR = value & (uint16_t)0xFF;
and read with:
while (USART_GetFlagStatus(USARTx, USART_FLAG_RXNE) == RESET);
return (uint16_t)(USARTx->DR & (uint16_t)0xFF);
But we don't get any data to our serial port, and yes the usart settings on the PC have been checked,
Any idea?
/Thanks
2015-09-30 12:43 AM
Replace this:
GPIO_InitStructure.GPIO_Mode = GPIO_AF_USART6; with this: GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; Also, are you sure you want theUSART_ClockInit stuff? Are you really using
USART in synchronous mode?2015-09-30 2:29 AM
In addition to the previous poster I'd like to highlight the following points.
First, I never used pullup/pulldown for UARTs. GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
The internal pullup resistors are weak, so it probably does no harm.
Second, you did not tell about the hardware you use. Check that nothing else is routed to those pins what interferes with UART operation. Some Discoveryboards are infamous for using up most of the useful pins.
Third, you can use a debugger to step into the initialization, and check that all config registers are properly set. You can also short the TX and RX pin externally, and check that you receive every byte you send.
And fourth, a scope is always useful to follow the signal through the hardware, and locate the issue.
2015-09-30 2:55 AM
You can't just mix up random constants and interfaces and hope they work.
/*Enable USART6 clock*/ RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART6, ENABLE); /*GPIO stuff*/ RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_GPIOC, ENABLE); GPIO_InitTypeDef GPIO_InitStructure; //setup GPIO_InitStructure GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Fast_Speed; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init( GPIOC, &GPIO_InitStructure); /*Connect pins to alternate function, ie USART*/ GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_USART6); GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_USART6); /*Initialization of USART */ USART_InitTypeDef USART_InitStructure; //setup UART_InitStructure USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_Init(USART6, &USART_InitStructure); USART_Cmd(USART6, ENABLE);
2015-09-30 3:53 AM
2015-09-30 6:05 AM
The current code, a few of the previous errors were copy paste mistakes.
/*Enable USART6 clock*/
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART6, ENABLE);
/*GPIO stuff*/
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
GPIO_InitTypeDef GPIO_InitStructure; //setup GPIO_InitStructure
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Fast_Speed;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOC,
&GPIO_InitStructure);
/*Connect pins to alternate function, ie USART*/
GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_USART6);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_USART6);
/*Initialization of USART */
USART_InitTypeDef USART_InitStructure; //setup UART_InitStructure
USART_ClockInitTypeDef USART_ClockInitStructure; //setup UART_ClockInitStructure
USART_ClockStructInit(&USART_ClockInitStructure);
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_Init(USART6, &USART_InitStructure);
USART_ClockInit(USART6, &USART_ClockInitStructure);
USART_Cmd(USART6, ENABLE);
I'm running
STM32F4 Discovery with the expansion board STM32F4DIS-BB.
I use a RS232 cable connected at the base boards serial port and connect to the computer through an RS323 to usb adapter. The code doesn't crash or hang when writing. When I'm reading it stays at:
while
(USART_GetFlagStatus(USART6, USART_FLAG_RXNE) == RESET);
Any idea?
A note, I've tried running the code snippet you clive1 uploaded in this post:
/public/STe2ecommunities/mcu/Lists/STM32Discovery/DispForm.aspx?ID=10469&RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/%5bSTM32F4-Discovery%5d%20USART6%20Problem&Source=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder%3Dhttps%253a%252f%252fmy%252est%252ecom%252fpublic%252fSTe2ecommunities%252fmcu%252fLists%252fSTM32Discovery%252f%255bSTM32F4%252dDiscovery%255d%2520USART6%2520Problem%26FolderCTID%3D0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F%26currentviews%3D1006
whit the same result.2015-09-30 6:43 AM
Make sure HSE_VALUE and the PLL settings in system_stm32f4xx.c reflect the 8 MHz clock source used on the DISCO, make sure it's not set for the 25 MHz of the EVAL
2015-09-30 7:18 AM
The HSE_VALUE is 8 MHz.
As of PLL I'm not sure how to interpret it:#define PLL_M 8
#define PLL_N 336
/* SYSCLK = PLL_VCO / PLL_P */
#define PLL_P 2
/* USB OTG FS, SDIO and RNG Clock = PLL_VCO / PLLQ */
#define PLL_Q
I'll appreciate your help.
2015-09-30 7:31 AM
The ClockInit stuff is extraneous, you can lose it.
Check the jumpers on the STM32F4-DIS-BB to ensure PC6/7 get to the RS232 connector.Double check the cable if the USB-RS232 Dongle is not directly attached.2015-09-30 8:07 AM
Yes the jumpers JP1 and JP2 are set.
I'm starting to suspect that the cause may be on the PC side. I'll have the virtual com driver installed though and use a serial viewer with the correct USART settings.