cancel
Showing results for 
Search instead for 
Did you mean: 

SDHC support

lorenzo23
Associate II
Posted on March 09, 2010 at 00:09

SDHC support

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
lorenzo23
Associate II
Posted on May 17, 2011 at 13:42

..Nobody has used a SDHC card here?

swhite2
Associate III
Posted on May 17, 2011 at 13:42

I've had a 32GB SDHC card running just fine on our hardware but that's using SPI which is of no help to you.

Nickname12668_O
Associate II
Posted on May 17, 2011 at 13:42

Hi Lorenzo,

The SDIO Card driver available with the STM32 Standard Library supports all SD Card types including SD High Capacity.

Look at the SD_PowerON function and especially the ''SD_HIGH_CAPACITY'' mask.

Regards,

lorenzo23
Associate II
Posted on May 17, 2011 at 13:42

Thanks Maestro,

I didn't notice it!

I'm looking into it, thanks a lot.

Lorenzo