cancel
Showing results for 
Search instead for 
Did you mean: 

problem with virtual com port

dion
Associate II
Posted on March 29, 2012 at 11:33

Hello to all,

I have stm32-h107 board, i use eclipse and yagarto toolchain (my OS is windows7).

I want to use the feature usb on the go to establish communication with my laptop.

i downloaded the driver for virtual com port and installed it in my laptop. Afterwards, i compiled the example ''Virtual_COM_Port'' ( taken from ''STM32_USB-FS-Device_Lib_V3.3.0''), and compiling gave no errors. The problem rises as i start the debugging : code 43 pops up, that is ''Windows has stopped this device because it has reported problems''. I check Device Manager and there is an ''Unknown Device'' under Universal Serial Bus Controllers with an exclamation mark. I load to this device the inf file that i have already installed, but nothing changes.

Any ideas are welcome!

Best regards,

Dion
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
michaelp
Associate
Posted on March 29, 2012 at 14:21

You should write *.inf script file.Without this plug and play process does not work right

dion
Associate II
Posted on March 29, 2012 at 14:56

thank you very much for the reply! i am newbie so i lack of experience. i will implement your idea.

Best regards,

Dion