Problem with I2C-OLED interfacing
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-15 1:09 AM
I am trying to interface an I2C OLED display with an STM32L053C8 board. However, instead of using STM32CubeMX to initialize my different pins, I had to manually assign them, because the example programs which come along with the board, do not open on CubeMX. I think I have made some error in the initialization. When I run the program in the initialization of the oled( i.e SSD1306_Init() ) part, when it checks whether the device is ready, i.e
if (HAL_I2C_IsDeviceReady(&hi2c1, SSD1306_I2C_ADDR, 1, 20000) != HAL_OK)
it goes into this particular function and gets stuck in an infinite while loop. The part which causes it to get stuck is highlighted in the code.
((HAL_GetTick() - tickstart) > Timeout)) never satisfies.
If someone tells me what I have done wrong, it would be of great help.
HAL_StatusTypeDef HAL_I2C_IsDeviceReady(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint32_t Trials, uint32_t Timeout)
{ uint32_t tickstart = 0U;__IO uint32_t I2C_Trials = 0U;
if (hi2c->State == HAL_I2C_STATE_READY)
{ if (__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_BUSY) == SET) { return HAL_BUSY; }/* Process Locked */
__HAL_LOCK(hi2c);hi2c->State = HAL_I2C_STATE_BUSY;
hi2c->ErrorCode = HAL_I2C_ERROR_NONE;do
{ /* Generate Start */ hi2c->Instance->CR2 = I2C_GENERATE_START(hi2c->Init.AddressingMode, DevAddress);/* No need to Check TC flag, with AUTOEND mode the stop is automatically generated */
/* Wait until STOPF flag is set or a NACK flag is set*/ tickstart = HAL_GetTick(); while ((__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_STOPF) == RESET) && (__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_AF) == RESET) && (hi2c->State != HAL_I2C_STATE_TIMEOUT)) { if (Timeout != HAL_MAX_DELAY) { if ((Timeout == 0U) || ((HAL_GetTick() - tickstart) > Timeout)) { /* Device is ready */ hi2c->State = HAL_I2C_STATE_READY; /* Process Unlocked */ __HAL_UNLOCK(hi2c); return HAL_TIMEOUT; } } }- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-15 1:56 AM
What is the value of the SSD1306_I2C_ADDR macro ?
Make sure the I2C address is the 8-bit representation (0x78) and not the 7-bit one (0x3c) as it happens, for example, in the Arduino environment.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-15 4:49 AM
The address is 0x78. I manually added the I2C peripheral to my program. I feel like I may have missed something when I did this. Could you please walk me over the process of what exactly I have to do to interface a peripheral without using CubeMX.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-15 5:02 AM
Basically, this is what you need to do:
- Enable peripheral clock
- Enable GPIO clock
- Setup alternate functions
- If used, configure peripheral's interrupts and NVIC.
- Configure I2C with proper initialization settings
If you don't want to use CubeMX you can look, as a reference, to the examples provided in the Cube software package. E.g.: in the STM32L0 package I2C polling example can be found in:
Projects\STM32L053R8-Nucleo\Examples\I2C\I2C_TwoBoards_ComPolling
Look, in particular, to the HAL_I2C_MspInit() call.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-16 1:20 AM
I did something similar recently with a STM32F103 but took the opposite approach. I created a new project in CubeMX and added the code samples to that. You could at least generate the blank project and see how its initialisation differs from yours.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-17 11:15 PM
Hey, thank you so much for replying. apologies for the late reply. I was wondering if you could tell me how I am to import the example questions into CubeMX. Whenever I try loading it from Keil, it says that it can not open the xml file.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-18 1:13 AM
Sorry I don't use Keil. As I said I just started a new project in CubeMX. Then I did the IO assignments I needed and copy and pasted the sample code I had in to my project. I'm using Atollic TrueStudio.