cancel
Showing results for 
Search instead for 
Did you mean: 

Need help about USB OTG FS HOST

tgoin
Associate II
Posted on May 19, 2014 at 15:18

Hello all,

I'm searching about example for USB dialog with USB OTG connector.

I don't understand what are difference between HID, CDC & MSC ?

My project is dialog with a usb device which only response to me.

Please have you example, because all i found on WWW is uncomplete.

I'm working with CoIDE.

Big Thanks
This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
chen
Associate II
Posted on May 19, 2014 at 15:44

''I don't understand what are difference between HID, CDC & MSC ?''

First understand that USB is divided into Host and Device :

USB Host eg PC

USB Device eg Mouse, Memory Stick

''HID, CDC & MSC''

These are all USB Devices :

HID = Human Interface Device - eg mouse, keyboard or joystick

CDC = Communications Device Class - eg RS232 to USB adapter, Modem, Network adapter

MSC = Mass Storage Device - eg USB memory stick

ST have provided examples of all 3 in their library (driver) for UST OTG

http://www.st.com/web/en/catalog/tools/FM147/CL1794/SC961/SS1743/PF257882

Unless you have the specific Evaluation board that they have written are for, you will have to modify the demo(s) for your hardware.

''My project is dialog with a usb device which only response to me.''

Unfortunately, unless you pay for your own VID (vendor Identifier) and PID (product idenifier) this is not possible.

You will have to use the demonstration PID/VIDs

tgoin
Associate II
Posted on May 20, 2014 at 11:20

Ok,

I need Device USB HID.

I downloaded library you say, but i don't see how send & received data !!!

In examples, it's always light led but never dialog with device :(

I'm working with stm32F4 discovery board.

I detect correctly the device connection but after i'm stoped ...

My device send his configuration, but i don't know which API used to read it.
chen
Associate II
Posted on May 20, 2014 at 11:51

''I need Device USB HID.

I'm working with stm32F4 discovery board.''

OK, it becomes a little easier. Download this :

http://www.st.com/web/en/catalog/tools/PF257904#

Build and load the example in

'stsw-stm32068.zip\STM32F4-Discovery_FW_V1.1.0\Project\Demonstration'

This has a simple HID. It uses the MEMS (accelerometers) on the eval board to simulate a USB HID mouse.

Study the example.

Work out how the MEMS data is transfered into the USB HID driver.

(Hint look at USBD_HID_GetPos() and USBD_HID_SendReport() )

tgoin
Associate II
Posted on May 20, 2014 at 15:40

Thanks for your answer,

but i don't understand.

There is always function/file not present.

I tried with Cube but generated code is also different library (hal ...) and i don't know enable irq with that.

chen
Associate II
Posted on May 20, 2014 at 16:02

''I'm working with CoIDE.''

''Thanks for your answer,

but i don't understand.

There is always function/file not present.''

I am afraid your IDE is the problem. The examples ST provide all work for

IAR

Atollic

Keil

You can download a free version of IAR (code size limited):

http://www.iar.com/Service-Center/Downloads/

I do not know if the demo project will work (fits in the limited code size)

tgoin
Associate II
Posted on May 20, 2014 at 18:40

I try again,

because my project is very advanced, GPS implemented, fatfs SDCARD implemented...

Stay just my USB device ...

Thanks

tgoin
Associate II
Posted on May 21, 2014 at 09:35

I use this code : http://mikrocontroller.bplaced.net/wordpress/?page_id=1993

In main,
while
(1)

{

// Test ob USB-Verbindung zum PC besteht

if
(UB_USB_HID_GetStatus()==USB_HID_CONNECTED) {

// Ceck ob Daten per USB empfangen wurden

check=UB_USB_HID_ReceiveData(buf);

if
(check==RX_READY) {

// wenn Daten empfangen wurden

// als Echo wieder zurücksenden

UB_USB_HID_SendData(buf,HID_OUT_BUFFER_SIZE);

}

}

UB_USB_HID_GetStatus()
send
USB_HID_CONNECTED
only 1 time !!! after it send
USB_HID_Detached ??????
chen
Associate II
Posted on May 21, 2014 at 11:57

''I use this code : http://mikrocontroller.bplaced.net/wordpress/?page_id=1993'';

''
UB_USB_HID_GetStatus()
send
USB_HID_CONNECTED
only 1 time !!! after it send
USB_HID_Detached ??????
'' I am unfamiliar with this code and do not have the time to debug it for you/them. I know the code in http://www.st.com/web/en/catalog/tools/PF257904# 'stsw-stm32zip\STM32F4-Discovery_FW_V1.1.0\Project\Demonstration' works. I have personally tried it here with Atollic. Start with this example and start tinkering with it to understand it. That is the best I can do with my limited time.