Is it possible to disable FS USB OTG Tx interrupt?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-09-30 6:27 AM
Posted on September 30, 2015 at 15:27
Hi all,
STM32F4Discovery's uUSB connector is connected to the FS OTG of the MCU. As I can see separate Rx and Tx interrupts are only available for HS OTG peripheral. Is it possible (or how can I) disable only the Tx interrupt in FS mode where only 1 ISR is available? Thanks, David
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0