cancel
Showing results for 
Search instead for 
Did you mean: 

ili9163 spi LCD Help Please!

monta
Associate II
Posted on February 17, 2015 at 12:00

Hi guys , I wrote this simple code based on the ili9163 documentation and what what i found online of the arduino library writen for the same display , yet all what i was able to do is get the Background LED to light up the panel , nothing diplaying apart from that , here is my code:

#include <stm32f4xx.h>

#include <stm32f4xx_adc.h>

#include <stm32f4xx_gpio.h>

#include <stm32f4xx_rcc.h>

#include <stm32f4xx_spi.h>

#define CSPin GPIO_Pin_1

#define ResPin GPIO_Pin_2

#define AOPin GPIO_Pin_4

#define DatPin GPIO_Pin_5

#define ClkPin GPIO_Pin_3

#define VCCPin GPIO_Pin_6

#define BLPin GPIO_Pin_7

#define DatPS GPIO_PinSource5

#define ClkPS GPIO_PinSource3

#define Red 0x8000

GPIO_InitTypeDef GP_InitDef;

SPI_InitTypeDef SPI_InitDef;

void initGPIO(){

RCC->AHB1ENR |= RCC_AHB1Periph_GPIOB; // Clock enable for GPIOB.

GP_InitDef.GPIO_Pin = CSPin | ResPin | AOPin | BLPin | VCCPin;

GP_InitDef.GPIO_Mode = GPIO_Mode_OUT;

GP_InitDef.GPIO_OType = GPIO_OType_PP;

GP_InitDef.GPIO_PuPd = GPIO_PuPd_NOPULL;

GP_InitDef.GPIO_Speed = GPIO_Speed_25MHz;

GPIO_Init(GPIOB, &GP_InitDef);

GP_InitDef.GPIO_Pin = DatPin | ClkPin;

GP_InitDef.GPIO_Mode = GPIO_Mode_AF;

GPIO_Init(GPIOB, &GP_InitDef);

GPIO_PinAFConfig(GPIOB, ClkPS, GPIO_AF_SPI3);

GPIO_PinAFConfig(GPIOB, DatPS, GPIO_AF_SPI3);

}

void initSPI3() {

// Initialize SPI3.

SPI_InitDef.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2;

SPI_InitDef.SPI_CPHA = SPI_CPHA_1Edge;

SPI_InitDef.SPI_CPOL = SPI_CPOL_Low;

SPI_InitDef.SPI_DataSize = SPI_DataSize_8b;

SPI_InitDef.SPI_FirstBit = SPI_FirstBit_MSB;

SPI_InitDef.SPI_Mode = SPI_Mode_Master;

SPI_InitDef.SPI_NSS = SPI_NSS_Soft;

SPI_Init(SPI3, &SPI_InitDef);

SPI_Cmd(SPI3, ENABLE);

}

void writeCommand(uint16_t command){

GPIO_ResetBits(GPIOB, AOPin); // Set A0 D/C pin LOW for command select.

SPI_I2S_SendData(SPI3, command);

while(SPI_I2S_GetFlagStatus(SPI3, SPI_I2S_FLAG_BSY) == SET);

}

void writeData(uint16_t data){

GPIO_SetBits(GPIOB, AOPin); // Set A0 D/C pin LOW for data select.

SPI_I2S_SendData(SPI3, data);

while(SPI_I2S_GetFlagStatus(SPI3, SPI_I2S_FLAG_BSY) == SET);

}

void writeData16(uint16_t data){

GPIO_SetBits(GPIOB, AOPin); // Set A0 D/C pin LOW for data select.

SPI_I2S_SendData(SPI3, data>>8);

while(SPI_I2S_GetFlagStatus(SPI3, SPI_I2S_FLAG_BSY) == SET);

SPI_I2S_SendData(SPI3, data);

while(SPI_I2S_GetFlagStatus(SPI3, SPI_I2S_FLAG_BSY) == SET);

}

void setCoordinates(){

writeCommand(0x2A);

writeData(0x00);

writeData(05);

writeData(0x00);

writeData(50);

writeCommand(0x2B);

writeData(0x00);

writeData(32);

writeData(0x00);

writeData(32+50);

writeCommand(0x2C);

}

int main(void)

{

int index;

initGPIO();

initSPI3();

GPIO_SetBits(GPIOB, BLPin); // Set The background LED Pin high.

//

GPIO_ResetBits(GPIOB, ResPin);

for (index = 0; index < 50000; index++);

GPIO_SetBits(GPIOB, ResPin);

for (index = 0; index < 50000; index++);

GPIO_ResetBits(GPIOB, CSPin);

for (index = 0; index < 50000; index++);

//Start The LCD initializing.

writeCommand(0x01); //Software reset

for (index = 0; index < 50000; index++);

writeCommand(0x11); // Exit Sleep

for (index = 0; index < 10000; index++);

writeCommand(0x26); //Set default gamma

writeData(0x04);

for (index = 0; index < 5000; index++);

writeCommand(0xC0); //Set Power Control 1

writeData(0x1F);

for (index = 0; index < 5000; index++);

writeCommand(0xC1); //Set Power Control 2

writeData(0x00);

for (index = 0; index < 5000; index++);

writeCommand(0xC2); //Set Power Control 3

writeData(0x00);

writeData(0x07);

for (index = 0; index < 5000; index++);

writeCommand(0xC3); //Set Power Control 4 (Idle mode)

writeData(0x00);

writeData(0x07);

for (index = 0; index < 5000; index++);

writeCommand(0xC5); //Set VCom Control 1

writeData(0x24); // VComH = 3v

writeData(0xC8); // VComL = 0v

for (index = 0; index < 5000; index++);

writeCommand(0x38); //Idle mode off

for (index = 0; index < 5000; index++);

writeCommand(0x3A); //Set pixel mode

writeData(0x05);

for (index = 0; index < 5000; index++);

writeCommand(0x36); //Set Memory access mode

writeData(0x08);

for (index = 0; index < 5000; index++);

writeCommand(0x29); //Display on

for (index = 0; index < 5000; index++);

writeCommand(0x2C);//Memory Write

for (index = 0; index < 5000; index++);

//Display Something

int px;

setCoordinates();

for (px=0;px < 132; px++){

writeData16(Red);

}

return 0;

}

Any idea what Am I doing wrong ?? I appreciate it !!!
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
jj2
Associate II
Posted on February 18, 2015 at 17:32

While you expose your Lcd Controller - nothing is provided with regard to your graphic Lcd module.   Might that assist?  (i.e. many such displays require the introduction of a ''contrast voltage'' - although newer, more integrated controllers may now manage display contrast via software)

Usually - but not always - such displays have strict initialization requirements with timing being of great importance.  (that should be revealed w/in the controller's data manual)

Lastly - usually there is one pin dedicated to command/display data - you must insure it's correct use.  And one pin usually serves to ''strobe in'' the command or data - you must comply with that signal's ''set-up/hold & width'' requirements.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.